Question
STM32MP2 + Android 13: Android WebView blank screen / Surface Lost, Forcing relayout
- 1 reply
- 436 views
Board/SoC: STM32MP2
Android version: AOSP Android 13 (android-13.0.0_r82)
WebView: com.android.webview 109.0.5414.123 (prebuilt)
Renderer: GLES
Display: 1024×600 (landscape‑native) @ ~63 Hz
Opening an android webview intermittently causes a blank screen. Logs look like the following:
2025-07-30 11:38:13.515 1750-1750 OpenGLRenderer W Surface lost, forcing relayout
The webview never recovers from this state.
Also get the following logs if it is relevant:
2025-08-12 16:16:48.810 3475-3504 OpenGLRenderer E Unable to match the desired swap behavior.
I've also attached the logcat file
Thanks