Skip to main content
MBhin
Associate II
July 3, 2019
Solved

STM32MP157x-EVAL Populate the target and boot the image related issue

Hi ST Community,

I am trying to install the linux image on STM32MP157x-EVAL (as given in https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP1_boards/STM32MP157x-EV1/Let%27s_start/Populate_the_target_and_boot_the_image ), But i am getting issue related to LCD output after booting from SD-Card. well all steps are ok till flashing SD-Card i.e.

Flashing service completed successfully

But the issue is after booting from SD card, i am getting nothing on LCD, could anyone give me suggestion, what went wrong. Why i am not getting the UBoot splash screen.

P.S: b000 was used for flashing and b101 was used for booting from SD Card. and jumper settings are as JP3 [12], JP4[23], JP5[23].

Best Regards

This topic has been closed for replies.

3 replies

Olivier GALLIEN
ST Technical Moderator
July 3, 2019

Hi,

Could please get and send the UART console log during boot ?

Thx

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
MBhin
MBhinAuthor
Associate II
July 4, 2019

hi,

it is

 NOTICE: CPU: STM32MP157AAA Rev.B
 NOTICE: Model: STMicroelectronics STM32MP157C eval daughter on eval mother
 NOTICE: Board: MB1263 Var1 Rev.C-01
 INFO: Reset reason (0x15):
 INFO: Power-on Reset (rst_por)
 INFO: Using SDMMC
 INFO: Instance 1
 INFO: Boot used partition fsbl1
 WARNING: Failed to access image id=28 (-2)
 ERROR: Partition ssbl not found
 PANIC at PC : 0x2ffdb96b
 
 Exception mode=0x00000016 at: 0x2ffda000

Thank you

Usman