Skip to main content
FinguPublic
Associate
September 12, 2024
Solved

STM32MP157F-EV1 - No boot log via ST-LINK.

tl,dr: No boot log or root term via ST-LINK connector on STM32MP157F-EV1. Haven't tried UART 4 yet.

This is related to:

https://community.st.com/t5/stm32-mpus-products/i-get-output-via-uart4-but-not-via-st-link-and-i-cannot-input/m-p/135067 

Reference: 

https://wiki.st.com/stm32mpu/wiki/How_to_get_Terminal 

The board: STM32MP157F-EV1

My host: Dell XPS, USB puck with two USB ports, running Ubuntu 22.04.4 LTS using Minicom 2.8.

Following

https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP1_boards/STM32MP157x-EV1/Let%27s_start/Populate_the_target_and_boot_the_image 

I have:

* successfully prog'd the microSD with the STM32MP1257F (note the "eff") firmware
  ie: FlashLayout_sdcard_stm32mp157F-ev1-optee.tsv
* the eval board boots to OpenSTLinux launcher
* all the demo apps will run

Just no log or root command line using the ST-LINK connector via USB. I cannot execute basic commands in

https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP1_boards/STM32MP157x-EV1/Let%27s_start/Execute_basic_commands 

My terminal command line is: sudo minicom -D /dev/ttyACM0.
Hardware flow control is off and UART settings are 115200 8N1.
Minicom does connect to ttyACM0.

I've ensured the Linux user is a part of the dialout group.

J1, J4, and J5 are set correctly.

I am respecting the power up and connection sequence described in user manual 6.7 Embedded ST-LINK/V2-1.  The LEDs are lit as described by the manual.

As the 'F' part is intended for secure device, as opposed to the 'C':

Does that 'F' load suppress terminal access? Shoud I try 'C'?

Or is something else going on?

 

This topic has been closed for replies.
FinguPublic
FinguPublicBest answer
Associate
September 12, 2024

Never mind.  Jumper config problem on my end.  Out of the box, UART4 is routed to the RS-232 DB9 connector.  You have to change those jumpers.

Dumb-ism on my end.  And not everybody reads-n-writes a language the same way.

This problem is solved.

2 replies

FinguPublic
Associate
September 12, 2024

Eh... I may have J4 and J5 backwards.  I will check this tomorrow (in my hemisphere).

FinguPublic
FinguPublicAuthorBest answer
Associate
September 12, 2024

Never mind.  Jumper config problem on my end.  Out of the box, UART4 is routed to the RS-232 DB9 connector.  You have to change those jumpers.

Dumb-ism on my end.  And not everybody reads-n-writes a language the same way.

This problem is solved.