Skip to main content
krjdev
Associate II
February 25, 2022
Question

STM32MP157F-DK2 support in mainline (vanilla) U-Boot

Are there any plans to support the STM32MP157F-DK2 board in mainline (vanilla) U-Boot?

It's supported in the ST fork from U-Boot, but with an older version from U-Boot from the year 2020.

Could also ask this in the U-Boot mailing list.

This topic has been closed for replies.

1 reply

Kevin HUBER
ST Employee
March 10, 2022

Hello @krjdev​ ,

The support of the mainline U-Boot is not planned for the moment.

I will come back to you if I have more information.

Regards,

Kevin

In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.