Skip to main content
Joel
Associate II
August 25, 2022
Solved

STM32MP157F-DK2 failing to boot on custom image

I'm targeting:

openstlinux-5.15-yocto-kirkstone-mp1-v22.07.27

DISTRO: openstlinux-eglfs

MACHINE: stm32mp15-disco

Image+SDK build fine. I create the raw file as usual, image SD card, and boot fails with:

NOTICE: Model: STMicroelectronics STM32MP157F-DK2 Discovery Board

NOTICE: Board: MB1272 Var4.0 Rev.C-02

INFO:   PMIC version = 0x20

INFO:   Reset reason (0x15):

INFO:     Power-on Reset (rst_por)

INFO:   FCONF: Reading TB_FW firmware configuration file from: 0x2ffe2000

INFO:   FCONF: Reading firmware configuration information for: stm32mp_io

INFO:   Using SDMMC

INFO:     Instance 1

INFO:   Boot used partition fsbl1

NOTICE: BL2: v2.6-stm32mp1-r1.0(debug):v2.6-dirty

NOTICE: BL2: Built : 13:14:26, Nov 23 2021

WARNING: CRC check failed on FWU metadata

WARNING: loading of FWU-Metadata failed, using Bkup-FWU-Metadata

WARNING: CRC check failed on FWU metadata

ERROR:  loading of Bkup-FWU-Metadata failed

PANIC at PC : 0x2ffea213

I have no troubles using dunfell release with machine `stm32mp1-disco`.

My kirkstone CI (fails to boot):

https://github.com/meta-flutter/meta-flutter/blob/kirkstone/.github/workflows/kirkstone-stm32mp15.yml

My known working

dunfell CI (works):

https://github.com/meta-flutter/meta-flutter/blob/dunfell/.github/workflows/dunfell-stm32mp15.yml

Running the STM1 starter images of the same variant does work. So something about the image config.

Any ideas?

This topic has been closed for replies.
Joel
JoelBest answer
Associate II
August 26, 2022

@Erwan SZYMANSKI​ 

It was the missing metadata.bin file. I had made my tests prior to adding the metadata.bin copy. The STMProg tool was failing looking for metadata.bin, so I had copied it for that; not realizing I just solved the problem.

Thanks for looking!

3 replies

Erwan SZYMANSKI
ST Technical Moderator
August 26, 2022

Hello @Community member​ ,

Thank you for your contribution !

Regarding your logs, TF-A has troubles with the metadata check for FWU as explained in this article.

However, i see that you updated your .yml file between Dunfell and Kirkstone with taking this into consideration with copying arm-trusted-firmware/metadata.bin too.

I will investigate and try to reproduce from my side, I will let you informed.

Kind regards,

Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Joel
JoelAuthorBest answer
Associate II
August 26, 2022

@Erwan SZYMANSKI​ 

It was the missing metadata.bin file. I had made my tests prior to adding the metadata.bin copy. The STMProg tool was failing looking for metadata.bin, so I had copied it for that; not realizing I just solved the problem.

Thanks for looking!

Erwan SZYMANSKI
ST Technical Moderator
August 28, 2022

Hi @Community member​ ,

Really glad to see that you were able to solve your issue !

Have a nice day !

Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.