Skip to main content
Associate
May 1, 2025 2:42 PM UTC
Solved

STM32MP157D-DK1 no ST-LINK detected on Windows

I have a new STM32MP157D-DK1.  I have booted the board using the enclosed SD card and all appears to be working.  The green LED next to CN6 is on, blue LED8 starts flashing a few seconds after power on.  One of the block of 4 red LEDs next to the ST-LINK connector is flashing.  I have connected the ST-LINK CN11 to a USB port on my Windows 11 laptop.  I was assuming that the ST-LINK would be detected by Windows and would appear in the list of devices.  However, I see nothing at all.  No ST-LINK, no virtual COM ports.  I have tried different power supplies for the board, different USB cables for the ST-LINK and different USB ports on the laptop.

Is there something else I need to do to see the ST-LINK or does this indicate the board might have a fault?

My aim was to run a very simple program on the CM4 processor using Cube IDE but so far all it says is No ST-LINK detected.  I have various other STM32 dev boards and the ST-LINK and COM ports show up just fine for all of those.

This topic has been closed for replies.
MB11Best answer
Associate
May 2, 2025 8:17 PM UTC

Turns out it was a faulty USB cable. In fact, several faulty cables.  Went through at least three before I found one that worked.

1 reply

MB11AuthorBest answer
Associate
May 2, 2025 8:17 PM UTC

Turns out it was a faulty USB cable. In fact, several faulty cables.  Went through at least three before I found one that worked.