Skip to main content
MHerz.1
Associate II
September 26, 2023
Solved

STM32MP157D-DK1 missing RAM

Hello, I'm currently working with a STM32MP157D-DK1 Development Board with 4GB DDR3L. I populated the board with a prebuild openstlinux 6.1 build like discribed in a guide in the ST wiki.

When checking the total memory i unfortunatly only get 407MB that are used.

 

root@stm32mp1:~# free --mega
 total used free shared buff/cache available
Mem: 407 138 152 13 140 269
Swap: 0 0 0

 

 Is there a way to use the complete 4GB of RAM?

 

Kind regards,

Markus

This topic has been closed for replies.
PatrickF
PatrickFBest answer
ST Employee
September 27, 2023

HI @MHerz.1 , 407MBytes sound normal. The memory is 4Gbits which is 512MBytes and some part are probably reserved for OpTee, DMA buffers and exchange buffers with Cortex-M4.

Regards

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent

2 replies

PatrickF
PatrickFBest answer
ST Employee
September 27, 2023

HI @MHerz.1 , 407MBytes sound normal. The memory is 4Gbits which is 512MBytes and some part are probably reserved for OpTee, DMA buffers and exchange buffers with Cortex-M4.

Regards

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
PatrickF
ST Employee
September 27, 2023

Few more details in dmesg

root@stm32mp1:~# dmesg | grep Memory:
[ 0.000000] Memory: 325492K/524288K available (12288K kernel code, 1371K rwdata, 3636K rodata, 1024K init, 235K bss, 133260K reserved, 65536K cma-reserved, 0K highmem)

Maybe look into this page (not fully related, but some interesting information about DDR mapping)
https://wiki.st.com/stm32mpu/wiki/How_to_configure_a_256MB_DDR_mapping_from_STM32_MPU_Distribution_Package#Introduction

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent