Visitor II
November 1, 2023
Question
STM32MP157C kernel 6.1 nand not working
- 2 replies
- 2369 views
I have developed a custom stm32mp157c board with a nand IC as storage using the FMC peripheral. This has worked fine with kernel v5.15, but I am trying to upgrade to kernel v6.1 due to driver related issues of the ethernet switch. However I can't seem to detect the mtd device anymore with the new kernel. I have done some digging and it seems it might be related to the new sys bus driver for the etzpc. The nand driver (FMC2) does currently not seem to load at boot.
Can anyone point me in the right direction? Is dit an issue with my devicetree or is there something wrong in de kernel.