Skip to main content
Dinesh K
Associate
October 2, 2021
Solved

STM32MP157C - How to Trigger USB Boot mode from OpenSTLinux Firmware

Hi ST Community,

We are using STM32MP157C-DK2 board and OpenSTlinux Firmware (v3.1-Openstlinux-5-4-dunfell-mp1-20-11-12) for our development. Currently for DFU from PC, we are triggering USB Boot mode by configuring Boot mode Switch (SW1) manually. But our product have a requirement to trigger USB boot mode from the running firmware automatically.

Is there any way to trigger USB Boot mode in STM32MP157C-DK2 board without any manual configuration ?

This topic has been closed for replies.
PatrickF
PatrickFBest answer
ST Employee
October 4, 2021

Hi,

please see this post : https://community.st.com/s/question/0D53W00000Mhm7zSAB/is-it-possible-to-trigger-a-usb-dfu-boot-from-a-running-stm31mp157cdk2-without-physical-switching-dips-etc

Regards.

In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent

2 replies

PatrickF
PatrickFBest answer
ST Employee
October 4, 2021

Hi,

please see this post : https://community.st.com/s/question/0D53W00000Mhm7zSAB/is-it-possible-to-trigger-a-usb-dfu-boot-from-a-running-stm31mp157cdk2-without-physical-switching-dips-etc

Regards.

In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
Dinesh K
Dinesh KAuthor
Associate
October 11, 2021

Hi @PatrickF​.

We followed the above post and able to trigger USB boot successfully.

Thanks for your support.