Associate
July 26, 2023
Question
STM32MP157C-DK2 LCD SPI works with V4.1.0 DevPackage but not with V5.0.0
- 7 replies
- 7210 views
Hello, I've just migrated from V4.1.0 dev package to V5.0.0 and the LCD SPI ilitek 9486 does not work anymore.
Configuration: STM32MP157A-DK1 with 3.5 LCD SPI touchscreen. Starter Package loaded with stm32mp157c-dk2 config. Linux kernel recompiled with ili9486 module and uploaded. Device tree file "stm32mp157c-dk2.dts" modified with spi5 added and display and uploaded.
Please, how can I do to recover the LCD SPI that worked on previsous dev package?