Skip to main content
Associate
June 19, 2024
Question

STM32MP157C-DK2 fails to flash the image on the board

os: Ubuntu (wsl)

I am trying to follow the steps as below:

https://wiki.st.com/stm32mpu/wiki/STM32MP15_Discovery_kits_-_Starter_Package#Installing_the_tools

However, step 6.2 Image flashing cannot be completed.

When I entered the command below, it iterated only for the tf-a-stm32mp157c-dk2-usb.stm32 file.

Here are printed messages.

root@jesong:/home/STM32MP157C-DK2/STM32MPU_workspace/STM32MP1-Ecosystem-v5.0.0/Starter-Package/stm32mp1-openstlinux-6.1-yocto-mickledore-mp1-v23.06.21/images/stm32mp1# STM32_Programmer_CLI -c port=usb1 -w flashlayout_st-image-weston/optee/FlashLayout_sdcard_stm32mp157c-dk2-optee.tsv
-------------------------------------------------------------------
STM32CubeProgrammer v2.16.0
-------------------------------------------------------------------

USB speed : High Speed (480MBit/s)
Manuf. ID : STMicroelectronics
Product ID : DFU in HS Mode @Device ID /0x500, @Revision ID /0x0000
SN : 0049002E3338510939303435
DFU protocol: 1.1
Board : --
Device ID : 0x0500
Device name : STM32MP15xx
Device type : MPU
Revision ID : --
Device CPU : Cortex-A7

Start Embedded Flashing service

Memory Programming ...
Opening and parsing file: tf-a-stm32mp157c-dk2-usb.stm32
File : tf-a-stm32mp157c-dk2-usb.stm32
Size : 220.40 KB
Partition ID : 0x01

Download in Progress:
[==================================================] 100%

File download complete
Time elapsed during download operation: 00:00:03.013

RUNNING Program ...
PartID: :0x01
Start operation done successfully at partition 0x01


Memory Programming ...
Opening and parsing file: tf-a-stm32mp157c-dk2-usb.stm32
File : tf-a-stm32mp157c-dk2-usb.stm32
Size : 220.40 KB
Partition ID : 0x01

Download in Progress:
[==================================================] 100%

File download complete
Time elapsed during download operation: 00:00:02.143

RUNNING Program ...
PartID: :0x01
Start operation done successfully at partition 0x01

I've also attached part of my log.

 

This topic has been closed for replies.

2 replies

PatrickF
ST Employee
June 20, 2024

HI @JE_SP 

strange to have twice TF-A load in the log file (maybe just because you tried twice).

Could you share the console log (using ST-Link USB which should show a VCP on your PC) ?

I see "Ubuntu (wsl)" , do this mean you are running Linux on a Windows WSL machine ?

Could you try Cubeprogrammer on a Windows machine or a Linux native machine ?

Regards

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
JE_SPAuthor
Associate
June 20, 2024

Hi, @PatrickF 

Thank you for your response.

I wrote to answer your question.

 

strange to have twice TF-A load in the log file (maybe just because you tried twice).

>> I think I wrote in a way that could lead to misunderstanding. (so I edited)
However, I entered that command only once.

 

Could you share the console log (using ST-Link USB which should show a VCP on your PC) ?

>> I already attached the log file, is there another way to get the log?

I got the log using "-log trace_optee.log" option.

Below is part of the contents of the file I attached.

07:50:12:005 -------------------------------------------------------------------
07:50:12:005 STM32CubeProgrammer v2.16.0
07:50:12:005 -------------------------------------------------------------------

07:50:12:005

07:50:12:005 Log output file: trace_optee.log
07:50:12:005 Command line: -c port=usb1 -w "flashlayout_st-image-weston/optee/FlashLayout_sdcard_stm32mp157c-dk2-optee.tsv" -log "trace_optee.log"
07:50:12:005
07:50:12:006
07:50:12:006
07:50:12:024 Device Descriptor:
07:50:12:024 |_bLength : 0x12
07:50:12:024 |_bDescriptorType : 0x01
07:50:12:024 |_bcdUSB : 0x0200
07:50:12:024 |_bDeviceClass : 0x00
07:50:12:024 |_bDeviceSubClass : 0x00
07:50:12:024 |_bDeviceProtocol : 0x00
07:50:12:024 |_bMaxPacketSize : 0x40
07:50:12:024 |_idVendor : 0x0483
07:50:12:024 |_idProduct : 0xdf11
07:50:12:024 |_bcdDevice : 0x0200
07:50:12:024 |_iManufacturer : 0x01
07:50:12:024 |_iProduct : 0x02
...

 

I see "Ubuntu (wsl)" , do this mean you are running Linux on a Windows WSL machine ?

>> Exactly Yes!!

 

Could you try Cubeprogrammer on a Windows machine or a Linux native machine ?

>> If my running in wsl could be causing the problem, I'll try again with the method you suggested.