Skip to main content
Associate
Mar 7, 2025 12:14 PM UTC
Question

STM32MP157 Memory Controller

Hi,

i have a question to the memory-controller and the supported memory-size.

I'm using the Part STM32MP157CAAx (Package: LFBGA448).

In the Datasheet (STM32MP157C/F) and AN5031 there is a definition to the supported SDRAM size.

For package "LFBGA448" the SDRAM is defined as following.

- DDR3/3L (16bits 533MHz) up to 1Gbyte., single rank.

My Questions:

a.) Does the Memory-Controller support a DDR3L (Configuration 512Meg x 16) with "Single-rank and Twin-Die?

b.) Does the Memory-Controller support the following Page sizes:

     - Page-Size= 2KB

     - Page-Size= 1KB (Page size per die)

Could you please give us support, to answer the questions.

Thank you.

Reguards

 

 

 

 

 

 

 

 

This topic has been closed for replies.

2 replies

Erwan SZYMANSKI
ST Technical Moderator
Mar 10, 2025 4:01 PM UTC

Hello @Fritz2 ,
According to DDR experts, there is no blocker to use a 1GB twin-die DDR3. No specific balling and internal ZQ connected to GND for the second die.

Concerning page sizes, the standard is 2K that switches into 1K for twin-die, but it should be transparent.

Do not hesitate to check the list of DDR validated on our side: https://wiki.st.com/stm32mpu/wiki/Validated_DRAM_on_STM32_MPU_portfolio

Kind regards,
Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Fritz2Author
Associate
Mar 11, 2025 9:08 AM UTC

Hello Erwan SZYMANSKY,

thank you for the answer with a good and usefull information.

I have an additional question.

I think some configuration registers (SMT32CubeMX / DDRCTRL / DDRPHYC) ) must be set when using the MPU (STM32MP157CAAx) with 1GB twin-die DDR3.

I have read the AppNote AN5168 (How to configure DDR on STM32MP1 MPUs), but i can not find some informations how to setup a "twin-die DDR3".

Could you please help us with some support, to answer the questions.

Thank you.

Kind reguards,

Fritz