Skip to main content
CharlesBlanchard
Associate II
July 18, 2022
Solved

STM32MP151 - How to activate MCO ?

Hello, 

I'm trying to leverage the MCO capability of the STM32MP1, but I don't success. I want to have LSE on MCO1 and HSE on MCO2. 

I'm using TFA -> uboot -> linux and I can build with Yocto or Buildroot.

Which steps should be done during TFA, uboot and on Linux ? 

I have tried different combination but there is no behaviour.

Also, I'm only doing device tree configuration, maybe I'm missing something elsewhere.

I have seen following resource and I'm confused on the way to proceed because of the warning on MCO pins :

https://community.st.com/s/article/FAQ-STM32MP1-bring-up-troubleshooting-guide

Thanks for your input,

Best regards,

Charles B

This topic has been closed for replies.
Olivier GALLIEN
Olivier GALLIENBest answer
ST Technical Moderator
July 20, 2022

Hi @Community member​ ,

Wiith Ecosystem version DV3.x and earlier, CubeMX not handle properly MCO configuration in Uboot and kernel DTS, which lead to a deadlock.

This is what is mentionned as a classical pitfall in https://community.st.com/s/article/FAQ-STM32MP1-bring-up-troubleshooting-guide

From DV4.0 this configuration is properly manage and MCO configuration is done in OPTEE.

If you want to remains in DV3.x or earlier version the w/a consist in using a dummy driver to manage MCO config as per already describe in this post

https://community.st.com/s/question/0D50X0000BDox5VSQR/clock-output-on-mco1-pin-stm32mp157

Hope it help

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

2 replies

Olivier GALLIEN
Olivier GALLIENBest answer
ST Technical Moderator
July 20, 2022

Hi @Community member​ ,

Wiith Ecosystem version DV3.x and earlier, CubeMX not handle properly MCO configuration in Uboot and kernel DTS, which lead to a deadlock.

This is what is mentionned as a classical pitfall in https://community.st.com/s/article/FAQ-STM32MP1-bring-up-troubleshooting-guide

From DV4.0 this configuration is properly manage and MCO configuration is done in OPTEE.

If you want to remains in DV3.x or earlier version the w/a consist in using a dummy driver to manage MCO config as per already describe in this post

https://community.st.com/s/question/0D50X0000BDox5VSQR/clock-output-on-mco1-pin-stm32mp157

Hope it help

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
CharlesBlanchard
Associate II
July 25, 2022

Thanks for your answer. I will check what is the preferred solution in our case.

Regards,

Charles