Associate II
March 13, 2023
Question
STM32MP15 OPTEE Minimum DDR3
- 2 replies
- 1208 views
Hello,
I am having trouble booting OPTEE on a custom platform with 256MB of DDR3. The boot log is attached. I added some debug printfs and I can see that OPTEE freezes on 454 in core/arch/arm/kernel/boot.c. I believe this is the first time OPTEE starts paging so I am wondering if there is a minimum size that the DDR3 must be to work correctly? Any help would be greatly appreciated :) Thanks!