Skip to main content
Dat Tran
Senior II
January 15, 2024
Question

STM32MP15: How do we set I2C6 clock source ?

I am using STM32CubeMx to generate device tree:

I got these in uboot device tree:

&rcc {
st,clksrc=<
CLK_MPU_PLL1P
CLK_AXI_PLL2P
CLK_MCU_PLL3P
CLK_PLL12_HSE
CLK_PLL3_HSE
CLK_PLL4_HSE
CLK_RTC_LSE
CLK_MCO1_HSI
CLK_MCO2_DISABLED
>;
 
st,clkdiv = <
1 /*MPU*/
0 /*AXI*/
0 /*MCU*/
1 /*APB1*/
1 /*APB2*/
1 /*APB3*/
1 /*APB4*/
2 /*APB5*/
23 /*RTC*/
3 /*MCO1*/
0 /*MCO2*/
>;
 
st,pkcs = <
CLK_CKPER_HSE
CLK_FMC_ACLK
CLK_QSPI_ACLK
CLK_ETH_DISABLED
CLK_SDMMC12_PLL4P
CLK_DSI_DSIPLL
CLK_STGEN_HSE
CLK_USBPHY_PLL4R
CLK_SPI2S1_PLL3Q
CLK_SPI2S23_PLL3Q
CLK_SPI45_HSI
CLK_SPI6_HSI
CLK_I2C46_HSI
CLK_SDMMC3_PLL4P
CLK_USBO_USBPHY
CLK_ADC_CKPER
CLK_CEC_LSE
CLK_I2C12_HSI
CLK_I2C35_HSI
CLK_UART1_HSI
CLK_UART24_HSI
CLK_UART35_HSI
CLK_UART6_HSI
CLK_UART78_HSI
CLK_SPDIF_PLL4P
CLK_FDCAN_PLL4R
CLK_SAI1_PLL3Q
CLK_SAI2_PLL3Q
CLK_SAI3_PLL3Q
CLK_SAI4_PLL3Q
CLK_RNG1_LSI
CLK_RNG2_LSI
CLK_LPTIM1_PCLK1
CLK_LPTIM23_PCLK3
CLK_LPTIM45_LSE
>;
....
};
 
I can see I2C6 is using HSI for clock source, UART1,2,3,4... also use HSI.
 
In linux, when I open UART, then check register RCC_OCENSETR , HSI bit is 1, mean HSI is on. This is good.
but if I open I2C6 only,  check register RCC_OCENSETR, bit 1 now is 0, mean HSI is disable. But I2C6 work fine.
 
My question is, is there any where overwrite these values? My device has only uboot and linux, no trusted or optee... and I don't see any where reset these values yet.
 
 
 
 
This topic has been closed for replies.

1 reply

PatrickF
ST Employee
January 16, 2024

Hi @Dat Tran 

bit 1 of RCC_OCENSETR  is HSIKERON. Required to keep clock in xxx-Stop mode, but no impact when processor is running.
HSION is bit0

 

I assume HSIKERON is related to wakeup settings for used peripherals.

 

Note: Only OpTee is supported in latest OpenSTLinux ecosystem. We strongly advice to go in that way to benefit from future ecosystem updates.

 

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent