Skip to main content
debugging
Lead
October 5, 2023
Solved

STM32MP15 ECO 5.0.0 How to configure u-boot for discrete power (and disable PMIC)

Following this:

https://wiki.st.com/stm32mpu/wiki/How_to_configure_U-Boot_for_your_board 

As the default config used stm32_defconfig.

At the step make menuconfig disabled PMIC in device driver -> power  and  enabled regulator power .

Though, this  causes compile errors when building u-boot.

Created a defconfig file for the board but not a new vendor-board folder assuming just to base the board as a variant of existing ST board.  In other words using make stm32mp157a-board-mx_defconfig.

In the config file :

CONFIG_TARGET_ST_STM32MP15X=y

Does this need to be set to "n" in case of using a board based on the STM32MP1 ?

Is disabling PMIC in u-boot actually required to boot a discrete powered board ?

This topic has been closed for replies.
debugging
debuggingBest answer
Lead
October 5, 2023

Disabled both PMIC and regulator power and build was done and boot did not cause side effects. I wonder if that's ok ? Enabling both causes errors. Would enabling PMIC cause any issues ?

1 reply

debugging
debuggingAuthorBest answer
Lead
October 5, 2023

Disabled both PMIC and regulator power and build was done and boot did not cause side effects. I wonder if that's ok ? Enabling both causes errors. Would enabling PMIC cause any issues ?