Skip to main content
debugging
Lead
August 28, 2023
Solved

STM32MP15 ECO 5.0.0. Documentation does not provide a information how to create a new FIP

As in a different post, The TF-A build did not create the FIP binaries after deleting the FIP build folder.

This article does not describe how to create a new FIP binary. only how to update. very confusing !

The fiptool does provide a create function but its not listed as one the options in this page: very confusing !

How to configure TF-A

How to use the "Create" option ?

This topic has been closed for replies.
debugging
debuggingBest answer
Lead
September 16, 2023

Just use the FIP command to build the FIP.bin even it does not exists. works.

 

4 replies

Erwan SZYMANSKI
ST Technical Moderator
August 29, 2023

Hello @debugging ,
You are right, we have no complementary explanation for fiptool create command, aside of the fiptool help.

To use it, you just have to do:
fiptool create <name_of_fip>

Then, use fiptool update command to add the different binaries inside, following the article you mentioned.

Kind regards,
Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
debugging
debuggingAuthor
Lead
August 30, 2023

Thanks, this question was raised because the issue I have with the TF-A not creating the fip binaries, so I wonder how to do it manually, but the docs did not define it.

 

Erwan SZYMANSKI
ST Technical Moderator
August 30, 2023

@debugging ,
I understand. If my previous comment answered your question, please do not hesitate to close this topic with "accepted solution".

Kind regards,
Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
debugging
debuggingAuthorBest answer
Lead
September 16, 2023

Just use the FIP command to build the FIP.bin even it does not exists. works.