Skip to main content
Associate II
January 22, 2024
Solved

STM32MP135F - How to enable ETH2 using MII to connect Switch

We have designed 2 seperate boards, main board has STM32MP135FAE on board connected to Microchip LAN8742 via ethernet1 mac and it is working. second board is a network board and has Marvell 88E6185 switch on board. Ethernet2 mac on STM32MP135F is connected to Port9 at the Switch using MII. However, STM32MP135F is not enabling internal clock. And eth2 is not activated.

  • I have tried setting ETH clock at 25MHz, no luck.

I have attached my configuration files and clock settings and dmesg log.

Any idea what might be wrong on my configurations? 

This topic has been closed for replies.
PatrickF
PatrickFBest answer
ST Employee
January 24, 2024

Hi @skarayigit 

Maybe check the expected device tree is loaded during boot.

Is there some hint using Ethernet framework debug ?

https://wiki.st.com/stm32mpu/wiki/Ethernet_overview#How_to_trace_and_debug_the_framework

 

STM32MP13 discovery board provide 2 x Ethernet (See https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP1_boards/STM32MP135x-DK/Let%27s_start/Unpack_the_STM32MP135x-DK_board) , so you could give a look to the Starter Package Device tree : https://github.com/STMicroelectronics/linux/blob/v6.1-stm32mp/arch/arm/boot/dts/stm32mp135f-dk.dts

For HW concerns, see also AN5474 Getting started with STM32MP13x lines hardware development

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent

2 replies

PatrickF
PatrickFBest answer
ST Employee
January 24, 2024

Hi @skarayigit 

Maybe check the expected device tree is loaded during boot.

Is there some hint using Ethernet framework debug ?

https://wiki.st.com/stm32mpu/wiki/Ethernet_overview#How_to_trace_and_debug_the_framework

 

STM32MP13 discovery board provide 2 x Ethernet (See https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP1_boards/STM32MP135x-DK/Let%27s_start/Unpack_the_STM32MP135x-DK_board) , so you could give a look to the Starter Package Device tree : https://github.com/STMicroelectronics/linux/blob/v6.1-stm32mp/arch/arm/boot/dts/stm32mp135f-dk.dts

For HW concerns, see also AN5474 Getting started with STM32MP13x lines hardware development

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
Associate II
January 30, 2024

There was an issue with the script that is updating the dtb files in the image. It wasn't updating the files under fip folder therefore, the clocks weren't changing. Thank for the help and quick reply @PatrickF, eth2 is active now.