Skip to main content
Associate II
Dec 22, 2023 7:46 PM UTC
Question

STM32mp135f-dk custom uboot environment not saving properly

I have an STM32mp135f-dk board that I have been using openstlinux-6.1 to develop images on.

For my board, I made a custom device tree "iris.dtb" which I intend to use instead of the default "stm32mp135f-dk.dtb".

I ran into an interesting issue where u-boot on my board would not load the my modified uboot environment variables.

For context, the following is my flash layout file with the u-boot-env at address 0x00904400

 

 

#Opt Id Name Type IP Offset Binary
- 0x01 fsbl-boot Binary none 0x0 arm-trusted-firmware/tf-a-stm32mp135f-dk-usb.stm32
- 0x03 fip-boot FIP none 0x0 fip/fip-stm32mp135f-dk-optee.bin
P 0x04 fsbl1 Binary mmc0 0x00004400 arm-trusted-firmware/tf-a-stm32mp135f-dk-sdcard.stm32
P 0x05 fsbl2 Binary mmc0 0x00044400 arm-trusted-firmware/tf-a-stm32mp135f-dk-sdcard.stm32
P 0x06 metadata1 FWU_MDATA mmc0 0x00084400 arm-trusted-firmware/metadata.bin
P 0x07 metadata2 FWU_MDATA mmc0 0x000C4400 arm-trusted-firmware/metadata.bin
P 0x08 fip-a FIP mmc0 0x00104400 fip/fip-stm32mp135f-dk-optee.bin
PED 0x09 fip-b FIP mmc0 0x00504400 none
PED 0x0A u-boot-env ENV mmc0 0x00904400 none
P 0x10 bootfs System mmc0 0x00984400 st-image-bootfs-openstlinux-weston-iris-machine.ext4
P 0x11 vendorfs FileSystem mmc0 0x04984400 st-image-vendorfs-openstlinux-weston-iris-machine.ext4
P 0x12 rootfs FileSystem mmc0 0x05984400 st-image-weston-openstlinux-weston-iris-machine.ext4
P 0x13 userfs FileSystem mmc0 0x105984400 st-image-userfs-openstlinux-weston-iris-machine.ext4

 

 

On my target development board I created a symlink for the fw-util config so that fw_printenv and fw_setenv would work. I intend to ad this to a bbappend for u-boot-stm32mp.bb later on.

 

 

ln -s /etc/fw_env.config.mmc /etc/fw_env.config

 

 

I also had to modify the contents of fw_env.config.mmc as follows, otherwise fw_printenv prints the error "Cannot read environment, using default
Cannot read default environment from file". I'm not sure why this works but it does.

 

 

# Block device example
/dev/disk/by-partlabel/u-boot-env 0x0000 0x2000
/dev/disk/by-partlabel/u-boot-env -0x2000 0x2000

 

 Then I set my fdtfile as shown.

 

root@iris-machine:~# fw_setenv fdtfile=iris.dtb
root@iris-machine:~# fw_printenv fdtfile
fdtfile=iris.dtb

 

This configuration persists after rebooting so I know fw-util is working correctly and there is a persistent u-boot environment image somewhere.

Yet, when I reboot and get a uboot shell via serial port fdtfile has the following value.

 

U-Boot 2022.10-stm32mp-r1 (Oct 03 2022 - 19:25:32 +0000)

CPU: STM32MP135F Rev.Y
Model: STMicroelectronics STM32MP135F-DK Discovery Board
Board: stm32mp1 in trusted mode (st,stm32mp135f-dk)
Board: MB1635 Var1.0 Rev.E-02
DRAM: 512 MiB
optee optee: OP-TEE: revision 3.19 (afacf356)
Clocks:
- MPU : 1000 MHz
- AXI : 266.500 MHz
- PER : 24 MHz
- DDR : 533 MHz
Core: 260 devices, 40 uclasses, devicetree: board
WDT: Started watchdog with servicing (32s timeout)
NAND: 0 MiB
MMC: STM32 SD/MMC: 0, STM32 SD/MMC: 1
Loading Environment from MMC... OK
In: serial
Out: serial
Err: serial
Previous ADC measurements was not the one expected, retry in 20ms
****************************************************
* WARNING 500mA power supply detected *
* Current too low, use a 3A power supply! *
****************************************************

Net: eth0: eth1@5800a000, eth1: eth2@5800e000
Hit any key to stop autoboot: 0
STM32MP>
STM32MP>
STM32MP>
STM32MP> print fdtfile
fdtfile=stm32mp135f-dk.dtb

 

So it seems u-boot itself is not loading its own environment correctly and is returning to defaults after every boot. This forces me to change fdtfile manually after every boot, or rename my device tree blob in the /boot directory. 

I also tried the following, which appears to work at first glance.

 

STM32MP> setenv fdtfile iris.dtb
STM32MP> saveenv
Saving Environment to MMC... Writing to MMC(0)... OK
STM32MP> env save
Saving Environment to MMC... Writing to redundant MMC(0)... OK

 

But after a reboot, fdtfile returns to the default value.

So I created a development workspace for u-boot-stm32mp using dev tool as it generally described in this article.

https://wiki.koansoftware.com/index.php/Using_devtool_to_modify_recipes_in_Yocto

And I started looking at the stm32mp13_defconfig described int his article.

https://wiki.st.com/stm32mpu/wiki/U-Boot_overview#U-Boot_environment_variables

And in the first 10 lines I see this.

 

robo1340@yocto-build-machine:~/stm32mp1/build-openstlinuxweston-stm32mp13-disco/workspace/sources/u-boot-stm32mp$ head -10 configs/stm32mp13_defconfig
CONFIG_ARM=y
CONFIG_ARCH_STM32MP=y
CONFIG_TFABOOT=y
CONFIG_SYS_MALLOC_F_LEN=0x180000
CONFIG_ENV_OFFSET=0x900000
CONFIG_ENV_SECT_SIZE=0x40000
CONFIG_DEFAULT_DEVICE_TREE="stm32mp135f-dk"
CONFIG_SYS_PROMPT="STM32MP> "
CONFIG_STM32MP13X=y
CONFIG_DDR_CACHEABLE_SIZE=0x8000000

 

I fiddled around with these settings for a while and built a few images from them but none worked.

I also dd'd the block device where the uboot env should be and can see that there are uboot environment variables present. I searched though it and found the following lines.

 

fdtfile=stm32mp135f-dk.dtb
...
fdtfile=iris.dtb

 

Since the one set to iris.dtb is coming second, I assume the redundant uboot env is getting set but not the primary one.

I can see that I could just change CONFIG_DEFAULT_DEVICE_TREE to "iris.dtb" then rebuild my image and that would fix the immediate issue, but it wouldn't fix the more general issue of my not being able to save uboot environment variables as I expect I should.

I feel I have all the moving pieces in front of me but just can't figure out how to make them align now. Thank you for any additional guidance that can be given.

 

4 replies

mmichala
Associate III
Aug 9, 2024 1:46 PM UTC

Hi @robo1340 !

I am using the same stm32mp135f-dk. Where did you find that /etc/fw_env.config? According to fw_env.config.mmc file found in meta-st-stm32mp/recipes-bsp/u-boot/u-boot-fw-config-stm32mp it should be:

/dev/disk/by-partlabel/u-boot-env		-0x2000		0x2000
/dev/disk/by-partlabel/u-boot-env		-0x2000		0x2000
robo1340Author
Associate II
Aug 10, 2024 12:44 PM UTC

Hello @mmichala 

It has been a long time since I worked this issue. I seem to recall eventually just setting the CONFIG_DEFAULT_DEVICE_TREE in the stm32mp13_defconfig. I have since then moved to a different stm32mp135 board after getting my proof of concept work done on the development kit.

I don't recall exactly where I got the fw_env.config.mmc, it probably came from a uboot related recipe though.

Associate II
Dec 11, 2025 11:08 AM UTC

Hi @robo1340 ,

I m also facing the same issue.
Did you find how to replace the custom devicetree in the uboot environment.

Thanks & Regards

Ganesh.K

 

Associate
Jun 30, 2026 11:36 PM UTC

Im encountering a similar issue but I have more information to add. It seems if you have redundant uboot environmental variables section, there can be a mismatch between the environmental variables that uboot loads and the environmental variables fw_printenv loads. On my board, fw_setenv modifies whichever partitions is currently not active and then updates flags to let itself know that that is new active environment. When booting uboot, it just always loads one of the environments. So in this case it sounds like fw_printenv thinks the redundant environment section of flash is the active one while uboot disagrees.

I have not really found a fix for this mismatch in logic yet, but maybe my uboot isn’t aware of the other redundant location at all? That or there is just a fundamental mismatch between how ST uboot behaves with a redundant environmental partition and how fw_setenv behaves. Saving the environment twice in fw_setenv should write to both but you may actually have to make an update to a variable or it will not work.