Skip to main content
Associate II
Nov 24, 2024 10:03 PM UTC
Question

STM32MP135 UBOOT Splash Screen

Hi All,

I am working on enabling and testing the LCD (RGB666) and backlight (enable and pwm) functionality on my STM32MP1 platform in U-Boot. I have configured the necessary U-Boot options for LCD and video support, including backlight control and display configuration, but I would like some clarification and guidance on the following:

  • Is it possible to test the LCD display in U-Boot?
  • Can I use the lcdputs command for basic testing, such as writing simple text to the display? If so, how should it be used correctly?
  • How can I verify that the backlight is working in U-Boot?
  • Does U-Boot provide any commands (e.g., vidinfo) to check video or LCD configuration?

I created custom u-boot recipe and .cfg file, can you check the attached rar?

Regards

 

This topic has been closed for replies.