Skip to main content
Visitor II
Jul 2, 2025 8:11 AM UTC
Question

stm32mp135 boot stuck

NOTICE: CPU: STM32MP135F Rev.Y
NOTICE: Model: STMicroelectronics STM32MP135F-DK STM32CubeMX board - openstlinux-6.1-yocto-mickledore-mp1-v23.06.21
NOTICE: BL2: v2.8-stm32mp1-r1.0(release):custom()
NOTICE: BL2: Built : 15:38:01, Jul 2 2025
NOTICE: BL2: Booting BL32
I/TC: Early console on UART#4
I/TC:
I/TC: Embedded DTB found
I/TC: OP-TEE version: Unknown_3.19 (gcc version 12.2.0 (Buildroot 2021.11-4428-g6b6741b)) #1 Wed Jul 2 06:15:25 UTC 2025 arm
I/TC: WARNING: This OP-TEE configuration might be insecure!
I/TC: WARNING: Please check https://optee.readthedocs.io/en/latest/architecture/porting_guidelines.html
I/TC: Primary CPU initializing
I/TC: WARNING: All debug access are allowed
I/TC: Platform stm32mp1: flavor PLATFORM_FLAVOR - DT stm32mp135f-dk-mx.dts
I/TC: DTB enables console (non-secure)
▒_▒▒z`@`@▒▒ÿ▒▒▒▒▒▒▒▒▒▒▒zc`x@▒▒▒]▒▒▒▒▒▒▒▒▒▒▒@▒▒▒▒@▒▒▒@▒▒@▒▒▒▒▒z@xeeyybcb@\@▒▒▒▒@bac▒_▒▒z`@`@▒▒ÿ▒▒▒▒▒▒▒▒▒▒▒zc`x@▒▒▒]▒▒▒▒▒▒▒▒▒▒▒@▒▒▒▒@▒▒▒@▒▒@▒▒▒▒▒z@efdga`d@\@▒▒▒▒@a`c▒_▒▒z@▒▒▒▒▒▒▒@▒▒▒@▒▒▒▒▒▒▒▒▒@▒▒@▒▒▒▒▒▒@▒▒▒▒▒@▒▒▒▒▒▒▒▒▒@▒▒▒▒▒z@▒▒]▒▒▒z@▒▒▒▒▒▒▒▒@c^ay▒▒ۿ▒▒▒▒▒▒▒▒z@▒▒▒▒▒▒@▒▒@▒▒▒@▒ۿ▒▒▒߿dx▒@▒▒▒▒▒▒@X▒▒▒▒▒▒@▒▒@▒▒▒߿▒Y▒]▒▒▒▒@b`bb^a`]▒▒▒cb▒▒]▒a^a@X▒▒▒@`b@b`be@]@aezcxz``@[`y``Y▒▒▒z@▒▒▒cb▒▒ace▒@▒▒▒^▒▒▒▒▒▒z@▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒@▒▒▒cb▒▒ace▒]▒▒@▒▒▒cb▒▒▒ŝ▒@▒▒▒▒▒@]@▒▒▒▒▒▒▒▒▒▒▒]f^a]▒▒▒▒▒]▒▒▒▒▒▒▒▒▒▒]▒▒a]▒bc^`f^ba▒▒▒▒▒z@▒▒▒cb▒▒a@▒▒@▒▒▒▒▒▒▒@▒▒▒▒@X▒▒\▒▒▒cb▒▒ace▒]▒▒]▒▒Y▒▒▒▒z@@eab@▒ق▒▒▒▒▒@▒▒▒▒▒z@▒▒]▒▒▒z@▒▒▒▒▒▒▒▒@c^ay▒▒ۿ▒▒▒▒▒▒▒▒z@▒▒▒▒▒▒@▒▒@▒▒▒@▒ۿ▒▒▒߿dx▒@▒▒▒▒▒▒@X▒▒▒▒▒▒@▒▒@▒▒▒߿▒Y▒▒▒▒▒▒z]@▒▒▒@z@a```@▒▒▒]@▒▒▒@z@bff^e``@▒▒▒]@▒▒▒@z@bd@▒▒▒]@▒▒▒@z@ecc@▒▒▒▒▒▒▒z@@afc@▒▒▒▒▒▒▒\@be@▒▒▒▒▒▒▒▒\@▒▒▒▒▒▒▒▒▒▒z@▒▒▒▒▒▒▒▒z@@@▒▒▒▒▒▒▒@▒▒▒▒▒▒▒▒@▒▒▒▒@▒▒▒▒▒▒▒▒▒@Xcb▒@▒▒▒▒▒▒▒Y▒▒▒▒z@@`@▒ق▒▒▒z@@@▒▒▒cb@▒▒_▒▒▒z@`▒▒▒▒▒▒▒@▒▒▒▒▒▒▒▒▒▒▒@▒▒▒▒@▒▒▒^^^@▒▒▒▒z@@@@▒▒▒▒▒▒▒▒▒z@@@▒▒▒▒▒▒▒▒▒z@@@▒▒▒▒▒▒▒▒▒▒▒▒▒@▒▒▒@▒▒▒▒▒▒▒@`@▒▒@▒▒▒@``z``z``z``z``z``▒▒▒G▒@▒▒▒@▒▒▒@▒▒▒▒▒▒X]ayY▒▒▒z@@@▒▒@▒▒▒▒▒▒▒▒@▒▒▒▒▒^▒▒▒@▒▒▒@▒▒▒@▒▒@▒▒▒▒@▒▒▒▒▒▒▒▒z@@a@@`▒▒▒cb▒▒~@

 

 

What is the problem? At first, data comes out of the serial, but then breaks in the middle. How do I fix this?

 

This topic has been closed for replies.

1 reply

PatrickF
ST Employee
Jul 2, 2025 2:32 PM UTC

Hi @sangjulee 

this sound like a UART baud rate issue (issue on root clock frequencies).

At that time there is maybe optee reprogramming clocks differently than the one done by TF-A without re-init UARTs (that's my assumption, but I'm not expert on this).

 

You should check Device Tree consistencies in between all modules (tf-a, optee-os, u-boot and kernel) as any differences on same node declaration might create strange behavior.

Are you using a STM32MP135F-DK  board with custom SW ? Does it work with Starter Package ?

 

Maybe have a look to https://wiki.st.com/stm32mpu/wiki/How_to_compile_the_device_tree_with_the_Developer_Package 

Regards.

 

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent