Skip to main content
Ara.1
Associate III
January 4, 2021
Solved

stm32mp1 watchdog command line test

Hi All,

i am getting watchdog Device or resource busy in stm32mp1

root@mp1som:~# dmesg | grep watchdog

[   2.108020] iwdg 5a002000.watchdog: unable to set timeout value, using default

[   3.642347] iwdg 5a002000.watchdog: timeout skrinked to 1

[   3.647585] systemd[1]: Hardware watchdog 'STM32 Independent Watchdog', version 0

[   3.654887] systemd[1]: Set hardware watchdog to 30s.

root@mp1som:~# echo V > /dev/watchdog

-sh: can't create /dev/watchdog: Device or resource busy

root@mp1som:~#

This topic has been closed for replies.
Ara.1
Ara.1Best answer
Associate III
January 5, 2021

its working used following command

wdctl

4 replies

KnarfB
Super User
January 4, 2021

How did you build your image? What version? Changes / additions? What mp1som?

Ara.1
Ara.1Author
Associate III
January 4, 2021

Its customized image built using yocto, following distro is the details

NOTE: Resolving any missing task queue dependencies

Build Configuration:

BB_VERSION          = "1.42.0"

BUILD_SYS           = "x86_64-linux"

NATIVELSBSTRING     = "universal"

TARGET_SYS          = "arm-openstlinux_weston-linux-gnueabi"

MACHINE             = "stm32mp1som"

DISTRO              = "openstlinux-weston"

DISTRO_VERSION      = "2.7-snapshot-20210104"

TUNE_FEATURES       = "arm vfp cortexa7 neon vfpv4 thumb callconvention-hard"

TARGET_FPU          = "hard"

DISTRO_CODENAME     = "warrior"

GCCVERSION          = "8.%"

PREFERRED_PROVIDER_virtual/kernel = "linux-mp1som"

Olivier GALLIEN
ST Technical Moderator
January 5, 2021

Hi @Ara.1​ ,

Looks like you are using a custom environment ( warrior + basic boot chain from V1.2 ecosystem) on a custom design based on SOM.

I'm afraid this is too much custom to be efficiently supported in this community.

I you confirm you are using a part from SOM maker integrating STM32MP1, please be aware that the SOM maker supposed to be your favorite support contact.

If not please give more details in order we can provide relevant support.

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Ara.1
Ara.1AuthorBest answer
Associate III
January 5, 2021

its working used following command

wdctl