Skip to main content
Visitor II
Nov 20, 2024 8:11 PM UTC
Question

STM32MP1 u-boot watchdog driver clamps to a maximum of 32 seconds

Looking at the u-boot driver (drivers/watchdog/stm32mp_wdt.c), it seems to hard code the prescaler to /256.
There is no warning if the maximum timeout is set. The linux driver seems to handle values up to the maximum of 131 seconds. Is there some reason u-boot needs to do this when the hardware supports longer timeouts ?

 

static int stm32mp_wdt_start(struct udevice *dev, u64 timeout_ms, ulong flags)
{
	struct stm32mp_wdt_priv *priv = dev_get_priv(dev);
	int reload;
	u32 val;
	int ret;

	/* Prescaler fixed to 256 */
	reload = timeout_ms * priv->wdt_clk_rate / 256;
	if (reload > RLR_MAX + 1)
		/* Force to max watchdog counter reload value */
		reload = RLR_MAX + 1;
	else if (!reload)
		/* Force to min watchdog counter reload value */
		reload = priv->wdt_clk_rate / 256;
...

 

 

 

 

This topic has been closed for replies.

1 reply

Roger SHIVELY
ST Employee
Nov 22, 2024 8:19 PM UTC

Hello @dfoley 

 

This post has been escalated to the ST Online Support Team for additional assistance. 

 

We'll contact you directly.

 

Regards,

Roger