Skip to main content
Associate
Sep 22, 2025 1:56 PM UTC
Question

stm32mp1 sai synchronous slave

Hi

I have stm32mp157c in my custom board i connect sai2 to codec(tlv320aic), i config sai2a as master (WITHOUT MASTER CLK OUTPUT) and sai2b as synchronous slave, mclk for codec come from rcc mco1 and this is my dts:

 

 

sound {
// compatible = "audio-graph-card", "simple-audio-card";
compatible = "audio-graph-card";
label = "AUDIOcard1";

routing =
"Playback" , "MCLK",
"Capture" , "MCLK";
dais = <&sai2a_port &sai2b_port>;
status = "okay";
};

sai2a:audio-controller@4400b004{
status = "okay";

/* USER CODE BEGIN sai2a */
dma-names = "tx";
// #clock-cells = <0>;
clocks = <&rcc SAI2_K>;
clock-names = "sai_ck";
 
frame-master;
bitclock-master;
 
sai2a_port: port {
sai2a_endpoint: endpoint {
remote-endpoint = <&tlv320_tx_endpoint>;
format = "i2s";
};
};
/* USER CODE END sai2a */
};

sai2b:audio-controller@4400b024{
status = "okay";

/* USER CODE BEGIN sai2b */
dma-names = "rx";
st,sync = <&sai2a 2>; /* Set SAI2B as slave of SAI2A. */

clocks = <&rcc SAI2_K>, <&sai2a>;
clock-names = "sai_ck", "NCLK";
 
sai2b_port: port {
sai2b_endpoint: endpoint {
remote-endpoint = <&tlv320_rx_endpoint>;
format = "i2s";
};
};

codec: tlv320aic32x4@18 {
compatible = "ti,tlv320aic32x4";
reg = <0x18>;
clocks = <&rcc CK_MCO1>;
clock-names = "MCLK";
ldoin-supply = <&v3v3>;
reset-gpios = <&gpioi 0 GPIO_ACTIVE_LOW>;
#sound-dai-cells = <0>;
status = "okay";
port {
#address-cells = <1>;
#size-cells = <0>;
tlv320_tx_endpoint: endpoint@0 {
reg = <0>;
remote-endpoint = <&sai2a_endpoint>;
};
tlv320_rx_endpoint: endpoint@1 {
reg = <1>;
remote-endpoint = <&sai2b_endpoint>;
};
};
 
now my tx path is ok and i can play sound but rx path for capture has some issue when run arecord
board ># arecord -D hw:0,1 -f S16_LE -c 2 -r 44100 -d 5 test.wav
arecord: pcm_read:2151: read error: Input/output error


i see in rx path bitclock and word clock desn't generate (from stm32mp1)
how should i config dts for this situation that can have sai2a as master WITHOUT MASTER CLOCK OUT and sai2b as synchronous slave
i read this thread:
This topic has been closed for replies.

2 replies

Christophe Guibout
ST Technical Moderator
Sep 23, 2025 8:49 AM UTC

Hello @jacob-sorber,

 

According to my understanding of your DT, SAI provides FS and SCK, but not MCLK, which is provided by mco1 to the codec : I'am not sure we can consider SAI as master.

 

I would recommand to move frame-master and bitclock-master under the codec so it is fully master, and keep sai2b as slave of sai2a.

 

BR,

Christophe

 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Associate
Sep 24, 2025 9:11 AM UTC

Hi 
I have to use stm32mp1 as (sai2) as master beacause if set codec (tlv320)  as master it need a clock (MCLK) with special frequency that mco1 can't reproduce, (its (tlv320) drvier force mco1 to reproduce a clk and stm32mp1 mco1 can't be set to that value so mp1 hangs)

also in stm32h7 I  use this codec (tlv320) and connect sai2 and sai is master in tx and rx path  and everything is OK in capture and playback (but in baremetal)