Hi @Ara.1
Since your need seems to know if the last reset occurs because of POR of WDOG, something else seems more adapted to you.
I advise you to take a look in the sources of the TF-A at the function: "print_reset_reason"
This function is available in the file "plat/st/stm32mp1/bl2_plat_setup.c" and displays the reason of the reset by reading the register RCC_MP_RSTSCLRR
static void print_reset_reason(void)
{
uint32_t rstsr = mmio_read_32(stm32mp_rcc_base() + RCC_MP_RSTSCLRR);
if (rstsr == 0U) {
WARN("Reset reason unknown\n");
return;
}
INFO("Reset reason (0x%x):\n", rstsr);
if ((rstsr & RCC_MP_RSTSCLRR_PADRSTF) == 0U) {
if ((rstsr & RCC_MP_RSTSCLRR_STDBYRSTF) != 0U) {
INFO("System exits from STANDBY\n");
return;
}
This register is accessible from application, so you can read its value.
To make a test on your board, you can try to read the register by using devmem. Details to install and use it are on the wiki: https://wiki.st.com/stm32mpu/wiki/How_to_read_or_write_peripheral_registers#Installing_Devmem_on_your_target_board
The address to read is the one read in "print_reset_reason",
stm32mp_rcc_base() + RCC_MP_RSTSCLRR
on my board STM32MP157F-DK2 with the developer package, the address is:
#define RCC_BASE U(0x50000000)
+
#define RCC_MP_RSTSCLRR U(0x408)
So the final address is 0x5000408
Once you use devmem, you get the value like this:
Then you interpret this value by using the reference manual that details all the possible values: https://www.st.com/resource/en/reference_manual/rm0436-stm32mp157-advanced-armbased-32bit-mpus-stmicroelectronics.pdf#page=996
Hope it help you,
Regards,
Kevin
In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.