Skip to main content
bfh_dls
Associate II
September 29, 2020
Solved

STM32MP1: OpenOCD cannot halt all cores

I am currently working on a design based around the STM32MP157C (mounted in the Seeed SoM - STM32MP157C).

I am trying to connect to the M4 Core on the target but I cannot halt it. When I attempt to do it, the debugger can halt the A7 CPU0 but fails at stopping the A7 CPU1 (Error: timeout waiting for DSCR bit change).

The M4 is completely inaccessible.

When I try to access the cores from the OpenOCD telnet interface, I can list the targets and get the following output after issuing a reset halt command.

> reset halt
stlink_dap_op_connect(connect)
SWD DPIDR 0x6ba02477
Deferring arp_examine of STM32MP157CACx.cm4
Use arp_examine command to examine it manually!
Target not examined, will not halt after reset!
stlink_dap_op_connect(connect)
stlink_dap_op_connect(reconnect)
SWD DPIDR 0x6ba02477
SWD DPIDR 0x6ba02477
STM32MP157CACx.cpu0: ran after reset and before halt ...
STM32MP157CACx.cpu1: ran after reset and before halt ...
STM32MP157CACx.cm4: hardware has 6 breakpoints, 4 watchpoints
STM32MP157CACx.cpu0 rev 5, partnum c07, arch f, variant 0, implementor 41
target halted in Thumb state due to debug-request, current mode: Supervisor
cpsr: 0x800001f3 pc: 0x00010bbc
MMU: enabled, D-Cache: disabled, I-Cache: enabled
timed out while waiting for target halted
TARGET: STM32MP157CACx.cpu1 - Not halted
> targets
 TargetName Type Endian TapName State 
-- ------------------ ---------- ------ ------------------ ------------
 0 STM32MP157CACx.ap1 mem_ap little STM32MP157CACx.tap halted
 1 STM32MP157CACx.ap2 mem_ap little STM32MP157CACx.tap halted
 2 STM32MP157CACx.axi mem_ap little STM32MP157CACx.tap halted
 3 STM32MP157CACx.cpu0 cortex_a little STM32MP157CACx.tap halted
 4 STM32MP157CACx.cpu1 cortex_a little STM32MP157CACx.tap running
 5* STM32MP157CACx.cm4 cortex_m little STM32MP157CACx.tap reset

Before the command was issued, all targets but the cm4 were in the running state (the cm4 is always stuck in the reset state).

How can I access the core and load a program into it ?

Tool versions and configuration:

  • STM32CubeIDE 1.4.0 on Ubuntu 20.04 (I use the provided OpenOCD)
  • STlink V2 with the latest firmware
  • Debug connection: SWD at 1.8 MHz (higher clock rates result in communication failure due to electrical contraints, lower clock rates do not change the result)
  • Debug mode setup: Connect under reset, Enable debug in low power mode and Stop watchdog counter when halt are both enabled
This topic has been closed for replies.
Olivier GALLIEN
Olivier GALLIENBest answer
ST Technical Moderator
September 30, 2020

Hi @bfh_dls​ 

Yes I confirm. You need to boot in engineering mode.

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

3 replies

Olivier GALLIEN
ST Technical Moderator
September 29, 2020

Hi @bfh_dls​ ,

First please check it can not be due to well know issue described in this post :

https://community.st.com/s/question/0D53W00000G1PG8SAN/update-stm32cubeide-version-142-stopped-sending-firmware-to-mpu

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
bfh_dls
bfh_dlsAuthor
Associate II
September 29, 2020

I don't think so, I want to access only the M4 core and have not even configured anything to boot on the A7 cores.

I have been reading up on the boot modes, if I understand correctly, the only way to access the M4 with nothing running on the A7 cores is through engineering mode ? (we are currently not booting in engineering mode).

Olivier GALLIEN
Olivier GALLIENBest answer
ST Technical Moderator
September 30, 2020

Hi @bfh_dls​ 

Yes I confirm. You need to boot in engineering mode.

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.