Skip to main content
Associate
April 16, 2024
Solved

STM32MP1 ETH_PHY_INTN

Hello! I am developing a custom board based on STM32MP151C MPU (TFBGA 361pins) with a RMII Ethernet PHY, and I have a simple question regarding to the PHY interrupt signal -sorry if this is a duplicated question, I haven't found a related topic in the forum-.

Is it mandatory to route the PHY interrupt output signal to a ETH1_PHY_INTN pin (any of the pins with this alternate function available) to capture interrupts? I have checked evaluation boards, and:

  • MB1263 board (STM32MP157FAA1) uses PG0, which does not has ETH1_PHY_INTN as an AF
  • MB1272 board (STM32MP157CAC3) uses PA6, which does not has ETH1_PHY_INTN as an AF

If PHY interrupt pin can be routed to any MP1 interrupt-capable pin, what is the purpose of the ETH1_PHY_INTN alternate function?

Many thanks in advance. Regards,

This topic has been closed for replies.
Christophe Guibout
ST Technical Moderator
April 25, 2024

Hi @jmglez,

 

The purpose of ETH1_PHY_INTN is to catch event from PHY (plug/unplug, WoL....)

It is not mandatory to route ETH1_PHY_INTN signal : it is not done on both MP15 boards as you mentioned, but it's done with MP13 DK board (see ETH1_MDINT and ETH2_MDINT).
This signal is managed by optee and declared as wakeup_pins in pinctrl file (example for MP13) :

wakeup_pin_2: pins2 {

pinmux = <STM32_PINMUX('I', 3, GPIO)>;

};

BR,

Christophe

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

2 replies

Christophe Guibout
ST Technical Moderator
April 25, 2024

Hi @jmglez,

 

The purpose of ETH1_PHY_INTN is to catch event from PHY (plug/unplug, WoL....)

It is not mandatory to route ETH1_PHY_INTN signal : it is not done on both MP15 boards as you mentioned, but it's done with MP13 DK board (see ETH1_MDINT and ETH2_MDINT).
This signal is managed by optee and declared as wakeup_pins in pinctrl file (example for MP13) :

wakeup_pin_2: pins2 {

pinmux = <STM32_PINMUX('I', 3, GPIO)>;

};

BR,

Christophe

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
jmglezAuthor
Associate
April 25, 2024

Hi Christophe,

thanks for answering my questions.

 

I guess the example you mentioned gives WoL support on the device, as the PHY interrupt output signal is routed to MPU PI3 with WKUP2 function. I've also checked that the 2nd ETH interface in the MP153 DK board is using ETH2_PHY_INTN AF, which makes sense to me.

In case of MB1263 and MB1272 boards I mentioned at first, in which PHYs interrupt output signals are not routed to PHY_INTN, what is the purpose of connecting PHY's INT signals to those MPU GPIOs? I suppose the MPU Ethernet peripheral wouldn't be abled to catch events from PHY, right?

Best regards,