Skip to main content
debugging
Lead
August 6, 2024
Solved

STM32MP1 ECO Unused GPIO busy after gpioset

Kernel tree does not assign any driver to pin PZ2. After gpioset -c gpiochip11 2=1, the pins goes actually high (from low) but the gpioset program stalls. SSH at that moment into the device shows:

 

line 0: "PZ0" input
line 1: "PZ1" input
line 2: "PZ2" output consumer="gpioset"
line 3: "PZ3" input
line 4: "PZ4" input consumer="kernel"
line 5: "PZ5" input consumer="kernel"
line 6: "PZ6" input
line 7: "PZ7" input

 

Aborting CTRL-C/Z gpioset causes the device to be busy upon a next set.

Is there a way to set the pin and the client release itself as consumer of  GPIO pin to be able to change the pin later back to low?

 

root@stm32mp1:~# gpioset -c gpiochip11 2=1
^Z[1]+ Stopped gpioset -c gpiochip11 2=1
root@stm32mp1:~# gpioset -c gpiochip11 2=0
gpioset: unable to request lines on chip '/dev/gpiochip11': Device or resource busy

root@stm32mp1:~# gpioget -c gpiochip11 2
gpioget: unable to request lines: Device or resource busy

 

 

This topic has been closed for replies.
PatrickF
PatrickFBest answer
ST Employee
August 6, 2024

Hi @debugging 

according to https://wiki.st.com/stm32mpu/wiki/How_to_control_a_GPIO_in_userspace, it is needed to use CTRL+C (and not CTRL+Z which keep the gpioset process running in background, which block further ressource usage). I don't know why gpioset is working like that.

To force exit of gpioset immediately, you need to use '-t0'

gpioset -t0 -c gpiochip11 2=1

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent

3 replies

PatrickF
PatrickFBest answer
ST Employee
August 6, 2024

Hi @debugging 

according to https://wiki.st.com/stm32mpu/wiki/How_to_control_a_GPIO_in_userspace, it is needed to use CTRL+C (and not CTRL+Z which keep the gpioset process running in background, which block further ressource usage). I don't know why gpioset is working like that.

To force exit of gpioset immediately, you need to use '-t0'

gpioset -t0 -c gpiochip11 2=1

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
debugging
debuggingAuthor
Lead
August 7, 2024

Tank you very much.  this helps a lot. Perhaps good to add to the wiki.

PatrickF
ST Employee
August 7, 2024

wiki update is planned even if the listed CTRL+C works and this is more a libgpio v2 specificity (seems an intended behavior).
I think it is minor as only command line issue. In an application, behavior is more clean.

regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent