Skip to main content
NBhat.1
Associate III
November 30, 2020
Solved

STM32 MPUs Ecosytem Release V2.1 Distribution package not using device tree files from meta-st-stm32mp-addons.

I've been using Ecosystem v2.0 without any issues now. We decided to move to v2.1 recently, followed the instructions from https://wiki.st.com/stm32mpu/wiki/STM32MP1_Distribution_Package to get the latest package. Then, as I did before, followed the instructions from https://wiki.st.com/stm32mpu/index.php/How_to_create_your_own_machine to create the distribution for our custom board. But running bitbake-st-image-weston failed because it could not create project.dtb as the project.dts files were not copied from the meta-st-stm32mp-addons folder to their respective folders in tf-a, u-boot and kernel.

Has anything changed in v2.1 with regards to custom device tree file placement?

This topic has been closed for replies.
NBhat.1
NBhat.1Best answer
Associate III
December 1, 2020

This issue is now fixed.

Root cause: In Ecosystem v2.0 ENABLE_CUBEMX_DTB ?= "1" was set in the cubemx-stm32mp.bbclass, but in ecosystem v2.1 this macro is supposed to be set in machine.conf file. It is set to 0 in cubemx-stm32mp.bbclass.

3 replies

NBhat.1
NBhat.1Author
Associate III
November 30, 2020

I also noticed that when I ran this command

$> MACHINE=stm32mp1-<ProjectName> DISTRO=openstlinux-weston source layers/meta-st/script/envsetup.sh

It didn't give me an option to agree to EULA certificate and printed the following (with ecosystem 2.0 it sued to give an option to accept EULA and WITH_EULA_ACCEPTED said Yes)

Configuration files have been created for the following configuration:

   DISTRO           : openstlinux-weston

   DISTRO_CODENAME  : dunfell

   MACHINE          : stm32mp1-midmark

   BB_NUMBER_THREADS : <no-custom-config-set>

   PARALLEL_MAKE    : <no-custom-config-set>

   BUILDDIR         : build-openstlinuxweston-stm32mp1-midmark

   DOWNLOAD_DIR     : <disable>

   SSTATE_DIR       : <disable>

   SOURCE_MIRROR_URL : <no-custom-config-set>

   SSTATE_MIRRORS   : <disable>

   WITH_EULA_ACCEPTED: <no-custom-config-set>

NBhat.1
NBhat.1Author
Associate III
November 30, 2020

I upgraded my system to from ubuntu 16.04 LTS 18.04 LTS (as required by ecosystem v2.1) and restarted the whole process of distribution package. Now I do get EULA acceptance pop-up, but still the build fails because the custom device tree files from the addons are not linked in tf-a, u-boot and kernel source folders.

NBhat.1
NBhat.1AuthorBest answer
Associate III
December 1, 2020

This issue is now fixed.

Root cause: In Ecosystem v2.0 ENABLE_CUBEMX_DTB ?= "1" was set in the cubemx-stm32mp.bbclass, but in ecosystem v2.1 this macro is supposed to be set in machine.conf file. It is set to 0 in cubemx-stm32mp.bbclass.