Hi @mhd0425
Although I guess STLINK-V3MODS has not been specifically tested on STM32MP1 devices, all STLINKs flavors are compatible with STM32MP1 (assuming VDD=3.3V).
If you are interested only in Virtual Com Port, and depending on amount of product you will product, maybe there could be some cheaper solutions:
- use a cheap STM32 part to do only UART/USB bridge (I guess USB full-speed would be enough for VCP)
- use a dedicated UART/USB bridge component or cable (e.g. FTDI chips/cables)
For debugging, providing an STDC14 (or other) connector on your board would allows to use any external debuggers (STLINK or other) during development phase.
Regards.
In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent