Skip to main content
Rajesh Kannan Selvam
Visitor II
February 10, 2021
Question

Steps to generate publicKeyhash.bin via openssl or any crypto utility

We are using STM32MP157c-DK2 board. Using STM32MP_KeyGen_CLI tool generated public key, private key and publicKeyhash.bin. 

As mentioned in STM32 webpage, https://wiki.st.com/stm32mpu/wiki/KeyGen_tool

Hash public key contains the SHA-256 hash of the public key in binary format which generated by Gen tool.

Is there a way or steps to generate same publicKeyhash.bin (without using STM32 key_Gen tool) via openssl or any other crypto utility 

This topic has been closed for replies.

1 reply

Olivier GALLIEN
ST Technical Moderator
February 24, 2021

Hi @Rajesh Kannan Selvam​ ,

I recover this draft / not verified procedure in case it can help and give some pointers :

To generate the header, you need to follow the format given by the wiki https://wiki.st.com/stm32mpu/wiki/STM32_header_for_binary_files

The key and signature are stored in a raw binary format.

To extract raw public key from .pem file, I suggest you use the pycryptodome python module (https://pypi.org/project/pycryptodome/ ; https://pycryptodome.readthedocs.io/en/latest/, https://pycryptodome.readthedocs.io/en/latest/src/public_key/ecc.html)

First, use an openssl command to convert your .pem file into a .der one (pycryptodome doesn’t accept .pem files)

openssl ec -in privateKey.pem -outform der -out privateKey.der

Then, use this script as example:

-----------------------------------------------------------------------

from Cryptodome.PublicKey import ECC

def dump_buffer(buf,step=16,name=""):

print("%s (%d bytes):" % (name, len(buf)))

for i in range(0,len(buf),step):

print (" ".join(["%02X" % c for c in buf[i:i+step]]))

f = open('privateKey.der','rt')

key = ECC.import_key(f.read())

pubk = key.public_key()

dump_buffer(pubk.pointQ.x.to_bytes(),name="x")

dump_buffer(pubk.pointQ.y.to_bytes(),name="y")

from Cryptodome.Hash import SHA256

from Cryptodome.Signature import DSS

message = b'I give my permission to order #4355'

h = SHA256.new(message)

signer = DSS.new(key, 'fips-186-3')

signature = signer.sign(h)

dump_buffer(signature,name="signature")

-----------------------------------------------------------------------

Hope it help

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.