Skip to main content
JIrao.1
Associate
January 27, 2023
Question

Start M4 firmware automatically

Hi!

I am using STM32MP157C-DK2 and i want to start the coprocessor from bootloader (I have readed the wiki page). First, I have done it manually and everithing works fine:

  • I have changed kernel m4_rproc:
&m4_rproc{
	/*Restriction: "memory-region" property is not managed - please to use User-Section if needed*/
	mboxes = <&ipcc 0>, <&ipcc 1>, <&ipcc 2>;
	mbox-names = "vq0", "vq1", "shutdown";
	status = "okay";
 
	/* USER CODE BEGIN m4_rproc */
	memory-region = <&retram>, <&mcuram>, <&mcuram2>, <&vdev0vring0>,
			<&vdev0vring1>, <&vdev0buffer>, <&mcu_rsc_table>;
	interrupt-parent = <&exti>;
	interrupts = <68 1>;
	wakeup-source;
	st,auto-boot = <1>;
	/* USER CODE END m4_rproc */
 
	m4_system_resources{
		status = "okay";
 
		/* USER CODE BEGIN m4_system_resources */
		/* USER CODE END m4_system_resources */
	};
};
  • I have loaded the firmware and run bootcmd:
load mmc 0#bootfs 0xc2000000 core_communication_new_CM4.elf
rproc init
rproc load 0 0xc2000000 2827764
rproc start 0
run bootcmd

With this, I was able to start the coprocessor firmware.

Now, I want to do it automatically: every time the board boots I want the coprocessor firmware to start. I have read on the wiki page and edited the stm32mp15_st_common.h file:

#define CONFIG_EXTRA_ENV_SETTINGS \
	STM32MP_MEM_LAYOUT \
	STM32MP_BOOTCMD \
	STM32MP_PARTS_DEFAULT \
	BOOTENV \
	"m4fw_name=rproc-m4-fw.elf\0" \
 "m4fw_addr=0xc2000000\0" \
	"boot_m4fw=rproc init; rproc load 0 0xc2000000 2827764; rproc start 0\0" \
 "boot_m4_mmc0=if load mmc 0#bootfs 0xc2000000 core_communication_new_CM4.elf ; then run boot_m4fw; fi;\0" \
 "bootcmd=run boot_m4_mmc0; run bootcmd_mmc0\0"
	STM32MP_EXTRA \
	STM32MP_BOARD_EXTRA_ENV

But now, I do not know how to go on. ¿How can I compile it and get it on the board?

Thanks!

https://wiki.st.com/stm32mpu/wiki/How_to_start_the_coprocessor_from_the_bootloader

This topic has been closed for replies.

3 replies

Erwan SZYMANSKI
ST Technical Moderator
January 27, 2023

Hello @JIrao.1​ ,

In the wiki link you target, it is also mentioned that you have to recompile U-Boot after your modification.

Please find below 2 links that will help you to do it:

I hope that this information will help you.

Kind regards,

Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
JIrao.1
JIrao.1Author
Associate
January 31, 2023

Hi @Erwan SZYMANSKI​ thanks for your reply! :beaming_face_with_smiling_eyes:

I have read and followed the steps of the wiki page (how to cross compile with the distribution package):

  • I have created fip-stm32mp157c-core_communication_new-mx-trusted.bin file with the above settings.
  • I then copied the binary to the sda5 dedicated partition:

0693W00000Y9aCvQAJ.jpg

  • Finally, I have rebooted the board but the M4 firmware does not boot.

I do not know if the ${kernel_addr_r} is not correctly asigned or I have forgotten some step.

Can you help me?

Thanks!

Erwan SZYMANSKI
ST Technical Moderator
February 1, 2023

Hello @JIrao.1​ ,

Did you also check the information provided by this wiki link: https://wiki.st.com/stm32mpu/wiki/Linux_remoteproc_framework_overview#Remote_processor_-27early-27_boot ?

Kind regards,

Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.