Skip to main content
Associate
Sep 26, 2025 8:06 PM UTC
Question

soc:pin-controller-z@54004000 failed with error -22

Hello!

 

I am getting this error, and tried everything I think, getting this error:
root@br-elec-01011-mu-rvt70hsmnwc00:~# dmesg | grep error && ls -l /dev/ttySTM*
[ 1.286601] stm32mp157-pinctrl: probe of soc:pin-controller-z@54004000 failed with error -22

 

Not sure if it is ok or not. Main components seems to work fine. But I am new to this, so not sure if it can cause issues along the way.

 

 

This topic has been closed for replies.

2 replies

Olivier GALLIEN
ST Technical Moderator
Oct 9, 2025 9:12 AM UTC

Hi @mikel 

May you provide further context and information ? 

eg your Linux Device Tree. ( dtb is fine) 

Thx

Olivier 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
mikelAuthor
Associate
Oct 9, 2025 3:51 PM UTC

Interesting I've attached files originally but looks like I've made a mistake.
Attached the final dts and dtb files. kernel tf-a and u-boot