Skip to main content
Associate
February 13, 2024
Question

setting MMU on stm32mp157

Please show me a working example of setting up the MMU for STM32MP157D-EV1. and where to place the Translation table correctly (for cortex A7)

It is assumed that all data and program will be located in DDR memory, without using the OS

 

This topic has been closed for replies.

3 replies

PatrickF
ST Employee
February 14, 2024

HI @Roman Andronov 

MMU settings are automatically handled by our OpenSTLinux deliveries. You don't have (and you can't) setup it directly.

If you are playing bare-metal, please note that STMicroelectronics did not provide any bare-metal support on STM32MP15 series. You have to check with ST partners https://www.st.com/content/st_com/en/partner/partner-program.html?key=STM32MP&country=country#2 .

 

Nevertheless, as we provide bare-metal support on STM32MP13 series thru STM32CubeMP13 delivery.

https://www.st.com/en/embedded-software/stm32cubemp13.html

As this device use same Cortex-A7 (but single core only) and very close HW, maybe you could get some insight from this delivery.

Regards

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
Associate
February 14, 2024

The latest version of StmCubeMX does not correctly create a project for stm32mp13 bare-metal (for STM32MP135F-DK)

 

there is no .cproject file with environment settings, as well as a linker file

The set of files that created the StmCubeMX

./mmu_test
./mmu_test/.mxproject
./mmu_test/Application
./mmu_test/Application/Core
./mmu_test/Application/Core/Inc
./mmu_test/Application/Core/Inc/cortex.h
./mmu_test/Application/Core/Inc/gpio.h
./mmu_test/Application/Core/Inc/main.h
./mmu_test/Application/Core/Inc/RTE_Components.h
./mmu_test/Application/Core/Inc/stm32mp13xx_hal_conf.h
./mmu_test/Application/Core/Inc/stm32mp13xx_it.h
./mmu_test/Application/Core/Src
./mmu_test/Application/Core/Src/cortex.c
./mmu_test/Application/Core/Src/gpio.c
./mmu_test/Application/Core/Src/irq_ctrl_gic.c
./mmu_test/Application/Core/Src/main.c
./mmu_test/Application/Core/Src/mmu_stm32mp13xx.c
./mmu_test/Application/Core/Src/stm32mp13xx_hal_msp.c
./mmu_test/Application/Core/Src/stm32mp13xx_it.c
./mmu_test/Application/Core/Src/system_stm32mp13xx_A7.c
./mmu_test/Drivers
./mmu_test/Drivers/CMSIS
--skip--
./mmu_test/Drivers/STM32MP13xx_HAL_Driver
--skip--
./mmu_test/mmu_test.ioc
./mmu_test/STM32CubeIDE
./mmu_test/STM32CubeIDE/.project
./mmu_test/STM32CubeIDE/.settings
./mmu_test/STM32CubeIDE/.settings/org.eclipse.core.resources.prefs

--end--

PatrickF
ST Employee
February 15, 2024
In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent