Skip to main content
Lukas1
Associate II
Jul 3, 2020 9:09 AM UTC
Solved

save linux image

Hi,

I want to make a backup of the SD-card with the linux image. I tried it with Win32 Disk Imager (like on the raspberryPi: https://thepihut.com/blogs/raspberry-pi-tutorials/17789160-backing-up-and-restoring-your-raspberry-pis-sd-card). Windows detects the SD-card, but it is not accessible in the file manager. There is no drive letter assigned :(

How can I save the image?

thanks in advance

regards, Lukas

This topic has been closed for replies.
Fee
FeeBest answer
Associate II
Jul 3, 2020 11:15 AM UTC

Hi,

we have the same issue lately. You can use some kind of virtual machine (e.g. the ubuntu vm you might have for building the software) and mount the SD-card in there or you can check out another windows program like DiskInternals Linux Reader (there is a free version, but just backups are possible with it).

My wild guess is that it might be some windows problem if you have it too but I'm no specialist in that.

Cheers

2 replies

Fee
FeeBest answer
Associate II
Jul 3, 2020 11:15 AM UTC

Hi,

we have the same issue lately. You can use some kind of virtual machine (e.g. the ubuntu vm you might have for building the software) and mount the SD-card in there or you can check out another windows program like DiskInternals Linux Reader (there is a free version, but just backups are possible with it).

My wild guess is that it might be some windows problem if you have it too but I'm no specialist in that.

Cheers

Lukas1
Lukas1Author
Associate II
Jul 3, 2020 12:09 PM UTC

Hi @Lukas Brückner​ ,

you saved my day :)

I made a backup of the image with DiskInternals Linux Reader. To flash the image to a new SD-card I used Win32 Disk Imager. Works great!:flexed_biceps: