Skip to main content
Charles Dias
Associate III
Jul 31, 2024 10:56 AM UTC
Solved

Run OP-TEE application on STM32MP157C-DK2 board

Dear,

I'm starting with OP-TEE on STM32MP15x line. I bring-up the board as described here and built the optee_example_hello_world as described here. However, I got the error code below:

TEEC_Opensession failed with code 0xffff0008 origin 0x3

Checking the boot messages, I realized that the profile system_services is used. This way, it is not possible to run any TA. 

So, is there any already compiled image for STM32MP157C-DK2 board that allows running a TA or do I have to modify the image to enable it? 

Thanks!

 

This topic has been closed for replies.

6 replies

Erwan SZYMANSKI
ST Technical Moderator
Jul 31, 2024 7:57 PM UTC

Hello @Charles Dias ,
Since OSTL v5.0, OP-TEE default configuration is non secure and loaded into DDR. It is mentioned here in OP-TEE overview : https://wiki.st.com/stm32mpu/wiki/OP-TEE_OTP_overview#OP-TEE_OS_configuration

So no, unfortunately we do not have an already compiled image that does what you want. You will have to recompile some components to load OP-TEE in SYSRAM, and activate secure_and_system_services profile.

Kind regards,
Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Associate
Nov 18, 2024 10:25 AM UTC

hello.

Sorry if I intrude on this post. It's not a relevant topic. I don't know who to turn to. I'm new to the forum and I need a little help.
I'm preparing the stm32mp157c-dk2 board with yocto project mickledore.

I have a problem compiling my Yocto for stm32mp157c-dk2 project. I run the bitbake command from build "bitbake -e core-image-minimal".
I get the error message: Error, the PACKAGE_ARCHS variable (all any noarch ${PACKAGE_EXTRA_ARCHS:tune-cortexa7}cortexa7 stm32mp157c_dk2) for DEFAULTTUNE (cortexa7) does not contain TUNE_PKGARCH ().Toolchain tunings invalid:
Tuning 'cortexa7' has no defined features, and cannot be used.

I tried to solve without success.
Anyone know how to solve it?

Thanks

Charles Dias
Associate III
Aug 6, 2024 12:00 PM UTC

Hi, @Erwan SZYMANSKI,

When I activate the secure_and_system_services profile, should I load the OP-TEE in SYSRAM or can I keep it on DDR even if it's not secure?

Thanks for your help!

 

Erwan SZYMANSKI
ST Technical Moderator
Aug 6, 2024 12:10 PM UTC

Hello @Charles Dias ,
Yes you need to put OP-TEE in SYSRAM on MP15 because this is the only memory secured for this series. 
On MP13, you can put OP-TEE in DDR for this same use case.

Kind regards,
Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
debugging
Lead
Aug 11, 2024 3:33 PM UTC

Yes you need to put OP-TEE in SYSRAM on MP15 because this is the only memory secured for this series.

For MP1 there are two modes and I managed to run them both:

1. With secure OP-TEE in SYSRAM and paging in DDR:

2. With unsecure OP-TEE in DDR

 

 

Charles Dias
Charles DiasAuthorBest answer
Associate III
Aug 8, 2024 1:55 PM UTC