Skip to main content
tzsolt
Associate II
January 19, 2022
Question

RGMII PHY connection doesn't come up 1000Mbps only 100Mbps

I use a STM32MP157C and connected to MAX24287 PHY by RGMII.

After linux booted there is only 100Mbps connection - I put the PHY into Diagnostic Loopback Mode and the situation is the same.

My dts:

&ethernet0{

pinctrl-names = "default", "sleep";

pinctrl-0 = <&eth1_pins_mx>;

pinctrl-1 = <&eth1_sleep_pins_mx>;

status = "okay";

/* USER CODE BEGIN ethernet0 */

phy-mode = "rgmii-id";

max-speed = <1000>;

phy-handle = <&phy0>;

 mdio0 {

#address-cells = <1>;

#size-cells = <0>;

compatible = "snps,dwmac-mdio";

reset-gpios = <&gpioa 4 GPIO_ACTIVE_LOW>;

reset-delay-us = <10000>;

post-reset-delay-us = <1000>;

phy0: ethernet-phy@3 {

    reg = <3>;

sfp;

/* compatible = "ethernet-phy-ieee802.3-c22"; */

/* interrupt-parent = <&gpioa>; */

/* interrupts = <9 IRQ_TYPE_EDGE_FALLING>; */

};

};

/* USER CODE END ethernet0 */

};

The PHY has 25MHz external clock, it gives 125MHz RX_CLK clock to the MAC, and the MAC would have give 125MHz TX_CLK (as GTX_CLK) to the PHY.

But with auto-negotiation the output on TX_CLK is only 25Mhz as 100Mbps.

This readable in the MAC registers:

devmem 0x50000A10 w 0x10800

devmem 0x50020004

0x00200000

devmem 0x500008FC

0x00000000

devmem 0x50000218

0x01004701

devmem 0x5800a000

0x0807E203

here ought to be 0x08072203 but the mac_speed_o[1] bit is "0" after negotiation.

Operating mode configuration register (ETH_MACCR)

Address offset: 0x0000

Reset value: 0x0000 8000

Bit 15 PS: Port Select

This bit selects the Ethernet line speed.

0: For 1000 Mbps operations

1: For 10 or 100 Mbps operations

In 10 or 100 Mbps operations, this bit, along with Bit 14, selects the exact line speed. In the

10/100 Mbps-only (always 1) or 1000 Mbps-only (always 0) configurations, this bit is readonly (RO) with appropriate value. In default 10/100/1000 Mbps configurations, this bit is readwrite (rw). The mac_speed_o[1] signal reflects the value of this bit.

Debug result from MAC registers:

0693W00000JMVe7QAH.jpg 

What could be the bad settings?

I could not have any idea more.

Thank you.

This topic has been closed for replies.

13 replies

OlivierK
ST Technical Moderator
February 8, 2022

Hi tzsolt  (Community Member)

Did you manage to progress on this issue?

fixed-linked is indeed used when mdio is not present to manage the phy.

The particularity of this device (Max24287) is that it is a parallel to serial interface between the Phy (SFP in your case) and the MAC so both sides need to be checked. I scanned through the Max24287 specifications, on the serial side, did you check the autonegociation in 1000 base x went well?

System software can configure the MAX24287 for 1000BASE-X auto-negotiation by setting PCSCR.BASEX=1 and BMCR.AN_EN=1.

Are you able to read those using the mdio bus?

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
tzsolt
tzsoltAuthor
Associate II
February 9, 2022

Unfortunatelly no progress...

Yes, I could read all of the registers and PCSCR.BASEX=1 and BMCR.AN_EN=1 are correct.

Meanwhile I figured out that there is one driver wrote by a guy but it is based on linux kernel 2.6 and now I downloaded 5.10.61 from ST.

We could not port it to 5.10...