Skip to main content
AVazquez
Associate III
Jun 26, 2025 6:09 AM UTC
Question

Reducing OP-TEE RAM size on STM32MP157C-DK2

Hi everyone,

I'm working with the STM32MP157C-DK2 board and trying to reduce the amount of RAM allocated to OP-TEE, but so far I haven't been successful.

There are 32MiB DDR dedicated for OP-TEE. 30MiB for TZSRAM and 2MiB for SHMEM.

In OP-TEE sources I changed value for CFG_TZDRAM_SIZE to 16 MiB and I'm keeping the value for SHMEM.

In TF-a sources I changed value for DDR_SEC_SIZE to 16MiB.

In Device tree I changed total RAM dedicated for OP-TEE to 18MiB.

But when kernel start I have a fail:

 

Starting kernel ...

E/TC:0 
E/TC:0 Core data-abort at address 0x2fff8762 (translation fault)
E/TC:0 fsr 0x00000207 ttbr0 0x2ffe0000 ttbr1 0x00000000 cidr 0x0
E/TC:0 cpu #0 cpsr 0x600001f3
E/TC:0 r0 0x2fff8762 r4 0x2ffe1f71 r8 0x00000073 r12 0xe0000000
E/TC:0 r1 0x2ffe1f1c r5 0x00000000 r9 0x00000000 sp 0x2ffe1e70
E/TC:0 r2 0x2ffd3355 r6 0x00000000 r10 0x2fff8762 lr 0x2ffcdf77
E/TC:0 r3 0x2fff8762 r7 0x2ffe1f71 r11 0x2ffe1f58 pc 0x2ffcd8f8
E/TC:0 TEE load address @ 0x2ffc0000
E/TC:0 Call stack:
E/TC:0 0x2ffcd8f8
E/TC:0 0x2ffcdf77
E/TC:0 Panic 'abort outside thread context' at core/arch/arm/kernel/abort.c:545 <abort_handler>
E/TC:0 TEE load address @ 0x2ffc0000
E/TC:0 Call stack:
E/TC:0 0x2ffc2499
E/TC:0 0x2ffcbb0b
E/TC:0 0x2ffc2101
E/TC:0 0x2ffc0b84

 

I’d like to ask if it’s actually possible to reduce the size of the reserved RAM for OP-TEE on this board, and if so, what would be the correct approach to do it?

 

This topic has been closed for replies.

2 replies

Olivier GALLIEN
ST Technical Moderator
Jun 27, 2025 4:01 PM UTC

Hi @AVazquez ,

 

I wonder if this article How to configure a 256MB DDR mapping from STM32 MPU Distribution Package - stm32mpu may not help you in your investigation ? 

 

Olivier 

 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
AVazquez
AVazquezAuthor
Associate III
Jul 1, 2025 6:45 PM UTC

Thanks, @Olivier GALLIEN 

I wasn’t aware of that article before. I’ve just read through it.

It refers to reducing the overall DDR mapping from 512 MB to 256 MB, not shrinking the memory specifically reserved for OP‑TEE.

 

Cheers!