Skip to main content
GLaure
Associate III
May 4, 2023
Question

Recipe for gcc-arm-none-eabi-native fails. Download checksum error with kirkstone.

I am puzzled with a curious build problem:

The recipe gcc-arm-none-eabi-native downloads gcc-arm-none-eabi-10.3-2021.10-x86_64-linux.tar.bz2 but the download finishes to early (at 100MB instead of 150MB). Therefore the checksum check fails.

BUT:

If I copy the SRC_URL:

SRC_URI = "https://developer.arm.com/-/media/Files/downloads/gnu-rm/10.3-2021.10/gcc-arm-none-eabi-10.3-2021.10-x86_64-linux.tar.bz2;name=gcc-arm-x86"

into a browser or use wget the download completes successfully. Also the sha256 sum is correct then.

Anyone experienced similar problems? Currently I will try to add a bbappend recipe to inject the archive as local file.

My systems:

Ubuntu 22.04 LTS

Alternatively docker container with 22.04

BB_NUMBER_THREADS="16" PARALLEL_MAKE="-j 16" bitbake gcc-arm-none-eabi-native
NOTE: Started PRServer with DBfile: /home/glaure/Development/SW_APP/nexio_tmp/ost-5.15/build/cache/prserv.sqlite3, Address: 127.0.0.1:41099, PID: 1439493
Loading cache: 100% |########################################################################################################| Time: 0:00:00
Loaded 4489 entries from dependency cache.
NOTE: Resolving any missing task queue dependencies
 
Build Configuration:
BB_VERSION = "2.0.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "ubuntu-22.04"
TARGET_SYS = "arm-ostl-linux-gnueabi"
MACHINE = "stm32mp1-nexio"
DISTRO = "openstlinux-weston"
DISTRO_VERSION = "4.0.4-snapshot-20230504"
TUNE_FEATURES = "arm vfp cortexa7 neon vfpv4 thumb callconvention-hard"
TARGET_FPU = "hard"
DISTRO_CODENAME = "kirkstone"
GCCVERSION = "11.%"
PREFERRED_PROVIDER_virtual/kernel = "linux-stm32mp"
meta-swupdate-nexio = "<unknown>:<unknown>"
meta-swupdate = "kirkstone:fb01170b98cf9541d286ba5a890fb85d83949b91"
meta-trionet 
meta-nexio 
meta-nexio-bsp = "<unknown>:<unknown>"
meta-python 
meta-oe 
meta-gnome 
meta-initramfs 
meta-multimedia 
meta-networking 
meta-webserver 
meta-filesystems 
meta-perl = "HEAD:05dcac98473402d87e0af73bbc2c5a6a840abe93"
meta-st-stm32mp = "HEAD:ca501bd7dbe023682903ceedddaacd940b0898f4"
meta-qt5 = "HEAD:5b71df60e523423b9df6793de9387f87a149ac42"
meta-st-openstlinux = "HEAD:cb736b403d0fef2a02390695613b6b4bb13ca1b7"
meta = "HEAD:f7766da462905ec67bf549d46b8017be36cd5b2a"
 
NOTE: Fetching uninative binary shim http://downloads.yoctoproject.org/releases/uninative/3.6/x86_64-nativesdk-libc-3.6.tar.xz;sha256sum=9bfc4c970495b3716b2f9e52c4df9f968c02463a9a95000f6657fbc3fde1f098 (will check PREMIRRORS first)
Initialising tasks: 100% |###################################################################################################| Time: 0:00:02
Sstate summary: Wanted 6 Local 0 Mirrors 0 Missed 6 Current 0 (0% match, 0% complete)
NOTE: Executing Tasks
WARNING: gcc-arm-none-eabi-native-10-r0 do_fetch: Checksum mismatch for local file /home/glaure/Development/SW_APP/nexio_tmp/ost-5.15/build/downloads/gcc-arm-none-eabi-10.3-2021.10-x86_64-linux.tar.bz2
Cleaning and trying again.
WARNING: gcc-arm-none-eabi-native-10-r0 do_fetch: Renaming /home/glaure/Development/SW_APP/nexio_tmp/ost-5.15/build/downloads/gcc-arm-none-eabi-10.3-2021.10-x86_64-linux.tar.bz2 to /home/glaure/Development/SW_APP/nexio_tmp/ost-5.15/build/downloads/gcc-arm-none-eabi-10.3-2021.10-x86_64-linux.tar.bz2_bad-checksum_c1d9dbf71e84d737a0e38fbf33c8f7f8b24519ee8b75a472af1873fd84769f8c
WARNING: gcc-arm-none-eabi-native-10-r0 do_fetch: Checksum failure encountered with premirror download of https://developer.arm.com/-/media/Files/downloads/gnu-rm/10.3-2021.10/gcc-arm-none-eabi-10.3-2021.10-x86_64-linux.tar.bz2;name=gcc-arm-x86 - will attempt other sources.
WARNING: gcc-arm-none-eabi-native-10-r0 do_fetch: Failed to fetch URL https://developer.arm.com/-/media/Files/downloads/gnu-rm/10.3-2021.10/gcc-arm-none-eabi-10.3-2021.10-x86_64-linux.tar.bz2;name=gcc-arm-x86, attempting MIRRORS if available

This topic has been closed for replies.

5 replies

GLaure
GLaureAuthor
Associate III
May 4, 2023

Fun fact: gcc-arm-none-eabi-native_10.bb is the only recipe having this issue.

My build fix:

gcc-arm-none-eabi-native_10.bbappend

FILESEXTRAPATHS:append := "${THISDIR}:"
 
SRC_URI = "file://files/gcc-arm-none-eabi-10.3-2021.10-x86_64-linux.tar.bz2 \
 "

GLaure
GLaureAuthor
Associate III
May 4, 2023

Got it:

The SRC_URL is replaced with: 'http://downloads.yoctoproject.org/mirror/sources/gcc-arm-none-eabi-10.3-2021.10-x86_64-linux.tar.bz2'

And the artifact there is different and much smaller.

Kevin HUBER
ST Employee
May 4, 2023

Hello @GLaure​ ,

I can confirm that the package size is not the same if you use the mirror link that you sent.

I will have a look why, but this is something handled by the community.

We can see in your log that it tried the correct link at first but failed to verify the crc.

If you look at the file in:

/home/glaure/Development/SW_APP/nexio_tmp/ost-5.15/build/downloads/gcc-arm-none-eabi-10.3-2021.10-x86_64-linux.tar.bz2_bad-checksum_c1d9dbf71e84d737a0e38fbf33c8f7f8b24519ee8b75a472af1873fd84769f8c

Is it complete?

If it is not the case, they was surely a problem with the site "developer.arm.com" or with your internet connection during the download of the package, because as you said, the one in :

https://developer.arm.com/-/media/Files/downloads/gnu-rm/10.3-2021.10/gcc-arm-none-eabi-10.3-2021.10-x86_64-linux.tar.bz2

is the correct one with the good checksum.

If the build tries to get the mirror tarball it is already not something normal.

Best Regards,

Kevin

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
Kevin HUBER
ST Employee
May 4, 2023

Hello @GLaure​ ,

In your build log, we can see that this is just a warning. Does the build continue after this warning?

Best Regards,

Kevin

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
GLaure
GLaureAuthor
Associate III
May 5, 2023

Now it does. I currently do not know if my bbappend recipe helps or not. I will look into it.

Bye Gunther