Skip to main content
Associate II
June 19, 2024
Question

Questions Regarding QuadSPI in STM32MP13 Bare Metal

Currently, I am testing QuadSPI.

Is it correct for the output to include Command / Address / Data?

I want to output only Data. While I can remove the Address through settings, I couldn't remove the Command.

Is it possible to output only Data?

This topic has been closed for replies.

2 replies

PatrickF
ST Employee
June 20, 2024

Hi @SL1 

QUADSPI is build to interface external Flash or similar.

For you concern, did you try playing with IMODE setting ?

PatrickF_0-1718895899603.png

Regards

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
SL1Author
Associate II
June 26, 2024

Hi, I recently solved this problem.

After checking, it was due to the ClockMode in the code below.

When I changed that part to XSPI_CLOCK_MODE_0, it worked correctly.

Is it correct that if it is set to XSPI_CLOCK_MODE_3, the address should be output before the data is output?

I will finish the post after confirming the answer.