Skip to main content
Ffu.1
Associate II
November 24, 2021
Question

Questions about burning erroI found the following errors when I burned kernel alone and starterpackage. May I ask why this was caused? The kernel is through https://github.com/STMicroelectronics/meta-st-stm32mp/blob/dunfell/recipes-kernel/linux/linux

I found the following errors when I burned kernel alone and starterpackage. May I ask why this was caused? The kernel is through https://github.com/STMicroelectronics/meta-st-stm32mp/blob/dunfell/recipes-kernel/linux/linux-stm32mp/README.HO W_to.txt teaching burn, Starterpackage is delivered via STM32_Programmer_CLI -c port= USb1 -w Flashlayout_st - image - weston/trusted/FlashLayout_sdcard_stm32mp157c - dk2 - trusted. TSV

This topic has been closed for replies.

11 replies

Tesla DeLorean
Guru
November 24, 2021

Please avoid putting the entire question in the Summary field, and that posted like are valid.

​

Complaining that generated image lacks a partition tables, so perhaps missing a step/stage of process, or not picking final file, but rather an intermediate one.​

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Ffu.1
Ffu.1Author
Associate II
November 25, 2021
I downloaded en. Flash-stm32mp1-openstlinux-5.10-dunfall-mp1-21-03-31.tar_v3.0.0.xz and burned its firmware. I don't know what middleware you mean. I re-uploaded flashlayout_sdcard_stm32mp157C-dk2-trusted. TSV and download log for you to see.
Olivier GALLIEN
ST Technical Moderator
November 24, 2021

Hi @Ffu.1​ ,

You flashlayout log looks a bit strange .. is it complete ?

Did you customized content of FlashLayout_sdcard_stm32mp157c-dk2 -trusted.TSV ?

Please clarify what you mean by "I burned kernel alone and starterpackage"

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Ffu.1
Ffu.1Author
Associate II
November 25, 2021
Dear Olivier:
Thank you help. Your reply to your question is as follows: ① I have re-sent you a complete flashout log as shown below; Flashlayout_sdcard_stm32mp157c-dk2-trusted.TSV I downloaded en. Flash-stm32mp1-openstlinux-5.10-dunfell-mp1-21-03-31.tar_v3.0.0.xz and burned its firmware. ③ I mean the following file error is caused by different SDK, one is in en.flash-stm32mp1-OpenStLinux-5.10-Dunfell-mp1-21-03-31.tar_v3.0.0. xz, which is the starter Package. Another error occurs when the kernel package compiled in developer-packageper is burned
Ffu.1
Ffu.1Author
Associate II
November 25, 2021
Ffu.1
Ffu.1Author
Associate II
November 25, 2021
Olivier GALLIEN
ST Technical Moderator
November 25, 2021

Hi @Ffu.1​ ,

Can you provide me exact reference of your DK board.

May you have another board available for a try ?

Thanks,

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Ffu.1
Ffu.1Author
Associate II
November 25, 2021

I find that sometimes it can be successfully burned and sometimes it is not successful. I don't know if it is the board problem. I don't know if you want to

Olivier GALLIEN
ST Technical Moderator
November 25, 2021

Hi @Ffu.1​ ,

What is your SDcard reference also ? Can you try another one ?

Seems you flash from Linux station ? Which OS ?

Thanks

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.