Skip to main content
Associate
Jul 28, 2026 6:50 AM UTC
Solved

Query Regarding Unused DSI and ANA Pins on STM32MP157FAC1

Hello,

We are designing a custom board using the STM32MP157FAC1 device. In our design, we are not using the DSI interface or the ADC peripheral.

We would like your guidance on the recommended handling of the corresponding unused pins.

(1.) DSI Interface:
Since the DSI interface is not used, how should the following differential signals be terminated ?
(a.) DSI_CKP / DSI_CKN
(b.) DSI_D0P / DSI_D0N
(c.) DSI_D1P / DSI_D1N

(2.) Analog Inputs:
As the ADC is not being used, what is the recommended way to connect or terminate the ANA0 and ANA1 pins ?

Could you please advise the recommended hardware implementation for these unused pins?

Regards,

PatrickF
PatrickFBest answer
ST Employee
Jul 29, 2026 9:16 AM UTC

Hi,

 

Please refer to AN5031 Table “Supply usage for unused features”

More generally, if not used:

  • DSI outputs should be left open
  • Analog inputs can be left open or grounded

 

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent

1 reply

PatrickF
PatrickFBest answer
ST Employee
Jul 29, 2026 9:16 AM UTC

Hi,

 

Please refer to AN5031 Table “Supply usage for unused features”

More generally, if not used:

  • DSI outputs should be left open
  • Analog inputs can be left open or grounded

 

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent