QSPI - NOR1 in TSV not detecting in STMCube programmer Tool
- 1 reply
- 1642 views
I have two NOR flash in my hardware.
- On SoM (Boot meadia detecting as NOR1 in Uboot)
- On Carrier Card
Both are detecting in Uboot as Nor0 and Nor1 but in STMCube programmer i am not able to flash to Nor1.
Tool given NOR1 not found error. So not able to flash to NOR1 and Boot from QSPI.
If i put NOR0 in tsv file it is flashing to carrier card NOr flash. I wanted to flash to On SoM QSPI which is detecting as NOR1 which is not supported in TSV file.
To test , I have made the carrier card SPI4 disabled then On SoM QSPI is detecting as NOR0 and flashing and booting works.
[2023-05-25 19:25:57] uboot> mtd list
[2023-05-25 19:26:01] SF: Detected is25wp016 with page size 256 Bytes, erase size 64 KiB, total 2 MiB
[2023-05-25 19:26:01] SF: Detected n25q256ax1 with page size 256 Bytes, erase size 64 KiB, total 32 MiB
[2023-05-25 19:26:01] List of MTD devices:
[2023-05-25 19:26:01] * nor0
[2023-05-25 19:26:01] - device: is25wp016@0
[2023-05-25 19:26:01] - parent: spi@4c002000
[2023-05-25 19:26:01] - driver: jedec_spi_nor
[2023-05-25 19:26:01] - path: /soc/spi@4c002000/is25wp016@0
[2023-05-25 19:26:01] - type: NOR flash
[2023-05-25 19:26:01] - block size: 0x10000 bytes
[2023-05-25 19:26:01] - min I/O: 0x1 bytes
[2023-05-25 19:26:01] - 0x000000000000-0x000000200000 : "nor0"
[2023-05-25 19:26:01] * nor1
[2023-05-25 19:26:01] - device: micron32mb@0
[2023-05-25 19:26:01] - parent: spi@58003000
[2023-05-25 19:26:01] - driver: jedec_spi_nor
[2023-05-25 19:26:01] - path: /soc/spi@58003000/micron32mb@0
[2023-05-25 19:26:01] - type: NOR flash
[2023-05-25 19:26:01] - block size: 0x10000 bytes
[2023-05-25 19:26:01] - min I/O: 0x1 bytes
[2023-05-25 19:26:01] - 0x000000000000-0x000002000000 : "nor1"
Please let me know how to resolve this issue.
Attached the STMCube programmer error and TSV file as .txt