Skip to main content
TStas.2
Associate II
March 11, 2022
Question

problem with own machine. DDR error

Hello 

I created own machine based of seeed module. 

at the strartup there is info 

NOTICE: CPU: STM32MP157CAC Rev.B
 
NOTICE: Model: STMicroelectronics custom STM32CubeMX board - openstlinux-5.10-dunfell-mp1-21-03-31
 
WARNING: VDD unknown
 
INFO: Reset reason (0x15):
 
INFO: Power-on Reset (rst_por)
 
INFO: FCONF: Reading TB_FW firmware configuration file from: 0x2ffe3000
 
INFO: FCONF: Reading firmware configuration information for: stm32mp_io
 
INFO: Using SDMMC
 
INFO: Instance 1
 
INFO: Boot used partition fsbl1
 
NOTICE: BL2: v2.4-r1.0(debug):v2.4-dirty
 
NOTICE: BL2: Built : 16:43:51, Nov 17 2020
 
INFO: BL2: Doing platform setup
 
INFO: RAM: DDR3-DDR3L 16bits 533000kHz
 
WARNING: Couldn't find property st,phy-cal in dtb
 
ERROR: DDR addr bus test: can't access memory @ 0xc0000004
 
PANIC at PC : 0x2ffedb39
 
 
 
Exception mode=0x00000016 at: 0x2ffedb39

I'm pretty new in linux on low lvl. Do anyone know where should i look for mistakes? Hardware is ok, i checked it on official image.

This topic has been closed for replies.

4 replies

OlivierK
ST Technical Moderator
March 14, 2022

Hello TStas.2 (Community Member)

When you say you checked the h/w on official image, then you can boot normally?

Otherwise it be worth looking at this article for exploring DDR issues.

STM32MP1 bring-up troubleshooting guide

FAQ: STM32MP1 how to validate the STM32MP1-DRAM connection on PCB, DDR test suite

Rgds,

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
TStas.2
TStas.2Author
Associate II
March 14, 2022

Yes i mean that all works ok

But i see

-Check configuration I2Cbus connection to STPMIC
I2C bus for pmic is done at early phase and raises a panic when the bus fails to be enabled.
In OpenSTLinux by default, TF-A expects STPMIC on I2C4. If this is not the case on your design device tree and TF-A code have to be modified.

In fact STPMIC is connected to I2C2. Maybe it will be solution. Tomorow i will check it. Thank You

OlivierK
ST Technical Moderator
March 23, 2022

Hi TStas.2 (Community Member)

Any progress with this issue? I guess you've already made the changes in TF-A regarding I2C2?

Regards,

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
TStas.2
TStas.2Author
Associate II
March 23, 2022

meanwhile i had different tasks, so i didn't focus 100% on that. But after changes i Have still some problem. Now i tryind test it step by step and compare with refference files. 

/PANIC at PC : 0x2fff08eb

Exception mode=0x00000016 at: 0x2fff08eb