Skip to main content
Associate III
July 11, 2024
Question

Problem configuring duty cycle in devicetree

Hello,
I am trying to configure a PWM in the boot process. I followed the steps in the documentation https://wiki.st.com/stm32mpu/wiki/TIM_device_tree_configuration .

I configured the pwmleds node

pwmleds {
		compatible = "pwm-leds";
		example {
			label = "stm32-pwm-leds-example";
			/* Use pwm1 channel 0 (e.g. TIM1_CH1) */
			/* period in nanoseconds (500000), normal polarity (0) */
			pwms = <&pwm1 0 30518 0>;
			max-brightness = <255>;
		};
	};
/* PWM DT provider on TIM1: "pwm1" */
&timers1 {
	status = "okay";
	/* spare all DMA channels since they are not needed for PWM output */
	/delete-property/dmas;
	/delete-property/dma-names;
	/* define pwm1 label */
	pwm1: pwm {
		/* configure PWM pins on TIM1_CH1 */
		pinctrl-0 = <&pwm1_pins_a>;
		pinctrl-1 = <&pwm1_sleep_pins_a>;
		pinctrl-names = "default", "sleep";
		/* enable PWM on TIM1 */
		status = "okay";
	};
};

I run the command cat /sys/kernel/debug/pwm
I see the next line
pwm-0   (example             :( requested enabled period: 30518 ns duty: 0 ns polarity: normal


The period is OK, but the  duty cycle is 0, so  basically the signal is always low.

How can I configure the duty cycle in the devicetree if I want to have the pwm working well in  the boot process?

I am in the 6.1 kernel version in the mickledore branch.

 

Regards, @obedPH 

This topic has been closed for replies.

2 replies

PatrickF
ST Employee
July 12, 2024

Hi @obedPH 

I fear PWM cannot put in 'run' only by Device Tree settings, which is mostly HW configuration.

You need to use it thru the framework.

https://wiki.st.com/stm32mpu/wiki/PWM_overview

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
obedPHAuthor
Associate III
July 15, 2024

Hi, @PatrickF , thank you for your response.

I see. I'm trying something different. I'll give you more context. I am using a MuRata module for the wifi in a custom PCB with a STM32MP15, for several reasons I have to use a timer for the LPO pin, since I don't have more lsco available sources. I need to use a pwm timer before the brcmfmac starts in order to make the wifi module work properly. I modified the leds-pwm.c file and the PWM was working, bit it didn't work as I wanted,  because, apparently, it needs to start way before if I want my wifi module to bring on correctly. Now I am trying to modify the u-boot, I added this lines in the stm32mp157f-dk2.dts.

 

pwmleds {
 compatible = "pwm-leds";
 example {
 //label = "stm32-pwm-leds-example";
 /* Use pwm1 channel 0 (e.g. TIM1_CH1) */
 /* period in nanoseconds (500000), normal polarity (0) */
 pwms = <&pwm1 2 30518>;
 max-brightness = <255>;
 u-boot,default-brightness = <127>;
 };
	};

 

 I saw the /drivers/led/led_pwm.c and this file reads the u-boot,default-brightness attribute. The problem is, in the u-boot process, the pwm is not active.

 

Searching in the configuration files, I noticed that the configs/stm32mp15_defconfig does not have the LED_PWM = y line

 

CONFIG_SYS_I2C_STM32F7=y
CONFIG_LED=y
CONFIG_LED_GPIO=y
CONFIG_STM32_FMC2_EBI=y

 

It just has the LED_GPIO configured, so I suspect that this is the reason why the driver is not working, since I added some logs in the driver and I don't see those log messages during the boot process.

How should I configure the devicetree if I want to load that driver in the u-boot? I suspect that I have to edit the config node in the stm32mp157f-dk2-u-boot.dtsi file, because I can see some leds configurations there, but I don't know how:

 

// SPDX-License-Identifier: (GPL-2.0-or-later OR BSD-3-Clause)
/*
 * Copyright (C) 2024, STMicroelectronics - All Rights Reserved
 * Author: STM32CubeMX code generation for STMicroelectronics.
 */

/* For more information on Device Tree configuration, please refer to
 * https://wiki.st.com/stm32mpu/wiki/Category:Device_tree_configuration
 */

/* USER CODE BEGIN includes */
#include "stm32mp15-scmi-u-boot.dtsi"
/* USER CODE END includes */

/ {

 /* USER CODE BEGIN root */

 aliases{
 i2c3 = &i2c4;
 usb0 = &usbotg_hs;
 };

 config{
 u-boot,boot-led = "heartbeat";
 u-boot,error-led = "error";
 u-boot,mmc-env-partition = "u-boot-env";
 //st,adc_usb_pd = <&adc1 18>, <&adc1 19>;
 st,fastboot-gpios = <&gpioa 13 (GPIO_ACTIVE_LOW | GPIO_PULL_UP)>;
 st,stm32prog-gpios = <&gpioa 14 (GPIO_ACTIVE_LOW | GPIO_PULL_UP)>;
 };

 led{

 led-red{
 label = "error";
 gpios = <&gpioa 13 GPIO_ACTIVE_LOW>;
 default-state = "off";
 status = "okay";
 };
 };
 /* USER CODE END root */

}; /*root*/

/* USER CODE BEGIN addons */

&pmic {
 u-boot,dm-pre-reloc;
};

&uart4{
 u-boot,dm-pre-reloc;
};

&usbotg_hs{
 u-boot,force-b-session-valid;
};

&uart4_pins_mx {
 u-boot,dm-pre-reloc;
 pins1 { /* UART4_RX */
 u-boot,dm-pre-reloc;
 /* pull-up on rx to avoid floating level */
 bias-pull-up;
 };
 pins2 {
 u-boot,dm-pre-reloc;
 };
};

 

 

Regards, @obedPH