Porting TF-A firmware to a custom stm32mp157a board does not boot
- 3 replies
- 1671 views
My custom board is based on stm32mp157a-dk1,remove the pmic and usb type c circuit,
My porting steps are as follows:
1. porting u-boot, verify that u-boot functions properly, compile the uboot trusted image, copy u-boot.dtb to FIP_artifacts/u-boot/ and rename it to u-boot-stm32mp157a-custom-trusted.dtb, copy u-boot- nodtb.bin to FIP_artifacts/u-boot/ and rename it to u-boot-nodtb-stm32mp15.bin
2. modify optie-os-stm32mp-3.12.0.r1-r0 source code, add custom dtsi and dts file, modify dtsi and dts file, add custom board in Makefile.sdk file CFG_EMBED_DTB_SOURCE_FILE, use make -f $PWD/ ... /Makefile.sdk CFG_EMBED_DTB_SOURCE_FILE=stm32mp157a-custom all command to generate tee-header_v2-stm32mp157a-custom.bin, tee-pageable_v2-stm32mp157a -custom.bin, tee-pager_v2-stm32mp157a-custom.bin three files and copied to the FIP_artifacts/optee/ directory, in the use of the command is an error prompt can not find other custom board related files in the FIP_artifacts/ directory, but can generate corresponding .bin files
3. Modify the tf-a source code, add custom device tree and custom-fw-config.dts, modify the corresponding device tree file, add custom board define in Makefile.sdk ,use make -f $PWD/... /Makefile.sdk -j8 TFA_DEVICETREE=stm32mp157a-custom TF_A_CONFIG=trusted ELF_DEBUG_ENABLE='1' all command to generate bl32 fwconfig folder and Copy the bl32 fwconfig folder to the FIP_artifacts/arm-trusted-firmware folder , use the command to generate the bl32 fwconfig folder with the error that some files under FIP_artifacts/ cannot be found, but it does not affect the generation of the bl32 fwconfig folder and corresponding files. fwconfig folder and the corresponding files
4. Use make -f $PWD/... /Makefile.sdk -j8 fip command to generate the fip-stm32mp157a-custom-trusted.bin and tf-a-stm32mp157a-custom-sdcard.stm32 firmware, using
sudo dd if=tf-a-stm32mp157a-custom-sdcard.stm32 of=/dev/sdb1 conv=fdatasync
sudo dd if=tf-a-stm32mp157a-custom-sdcard.stm32 of=/dev/sdb2 conv=fdatasync
sudo dd if=fip-stm32mp157a-custom-trusted.bin of=/dev/sdb3 conv=fdatasync
Synchronize the firmware and select the sd card to boot
As a result the serial port prints the following message.
PANIC at PC : 0x2fff2d17
Exception mode=0x00000016 at: 0x2fff2d17
The only thing I can guarantee is that u-boot has been successfully ported and working, other parts of the port only modify the device tree file, each part of the device tree are referred to the u-boot device tree to do cut, I hope someone can solve my problem!
Thank you very much!