Skip to main content
TTour.2
Visitor II
Nov 9, 2022 2:33 PM UTC
Question

Porting STM32MP1 on custom board : stuck at "Booting BL32", where to go next?

After following the wiki page "how to create your board device", I am exactly in the situation indicated at the end of this page : "The execution should fail just after the "Booting BL32" notice, because state definitions are missing in the device tree (in the pwr node overlay)".

For information, I don't use the Yocto (layers etc) env and the full OpenSTLinux distrib, but rather a custom buildchain and the ***-stm32mp-r2 sources (TF-A 2.4, U-boot 2020.10 & linux 5.10 with lightened conf). All of this works well on the EV-1 board using the associated ST conf (dts etc.) and I am now trying to port all that on a custom board.

In my porting task, I am then guessing the next step is to add custom-made conf in device trees, especially the pwr node. I would get inspiration from the EV-1 dts but my custom board does not have a PMIC as our stm32mp151 doesn't need to manage low power modes (which should make it more simple?), among other little differences.

Where could I find ressources / doc / training / guides/ examples of those next steps of board-specific configurations (pwr, rcc, clk...) ?

I think the AN5256 "discrete power supply" will help me along the way, as well as the embedded documentation in the source packages, but these are much less beginner-friendly than the wiki.st.com how-to guides.

This topic has been closed for replies.

1 reply

PatrickF
ST Employee
Nov 14, 2022 5:14 PM UTC

Hi @Théo Tourrès​ 

maybe this post might help you as pointing some places of examples of discrete power device tree.

https://community.st.com/s/question/0D53W00001pYs9XSAS/in-the-beal-environment-what-files-are-needed-to-generate-fip-after-compiling-optee

Regards,

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent