Skip to main content
Associate III
Jun 25, 2023 4:02 PM UTC
Question

OpenAmp_TTY_echo not creating rpmsg0|1

Hello,

Searched around but couldn't find a similar issue.Please point me to one if one exist. I have a custom board with the stm32mp157c mounted. Board works fine, trying to communication between the m4 and a7 processor using the rpmsg devices. I have the example compiled but when I run it either of the rpmsg0 or 1 devices are present under /dev. If I take a precompiled example of the tty echo it runs fine.

Log from my build
[40144.602678] remoteproc remoteproc0: powering up m4
[40144.612280] remoteproc remoteproc0: Booting fw image OpenAMP_TTY_echo_CM4.elf, size 2367104
[40144.623913] mlahb:m4@10000000#vdev0buffer: assigned reserved memory node vdev0buffer@10042000
[40144.631840] virtio_rpmsg_bus virtio0: rpmsg host is online
[40144.631970] virtio_rpmsg_bus virtio0: creating channel rpmsg-tty addr 0x400
[40144.644298] mlahb:m4@10000000#vdev0buffer: registered virtio0 (type 7)
[40144.650201] remoteproc remoteproc0: remote processor m4 is now up
[40144.656732] virtio_rpmsg_bus virtio0: creating channel rpmsg-tty addr 0x401

Log from the precompiled 

[40713.026976] remoteproc remoteproc0: powering up m4
[40713.031634] remoteproc remoteproc0: Booting fw image OpenAMP_TTY_echo.elf, size 217172
[40713.039020] mlahb:m4@10000000#vdev0buffer: assigned reserved memory node vdev0buffer@10042000
[40713.047833] virtio_rpmsg_bus virtio0: creating channel rpmsg-tty-channel addr 0x0
[40713.057806] virtio_rpmsg_bus virtio0: rpmsg host is online
[40713.063787] mlahb:m4@10000000#vdev0buffer: registered virtio0 (type 7)
[40713.070024] rpmsg_tty virtio0.rpmsg-tty-channel.-1.0: new channel: 0x400 -> 0x0 : ttyRPMSG0
[40713.077714] virtio_rpmsg_bus virtio0: creating channel rpmsg-tty-channel addr 0x1
[40713.086064] remoteproc remoteproc0: remote processor m4 is now up
[40713.098384] rpmsg_tty virtio0.rpmsg-tty-channel.-1.1: new channel: 0x401 -> 0x1 : ttyRPMSG1

The example source code is not modified. I am simply trying to first get it to run before making the changes that are needed for my use case.

Not sure where to start digging.

Thanks

This topic has been closed for replies.

1 reply

Erwan SZYMANSKI
ST Technical Moderator
Jun 27, 2023 11:51 AM UTC

Hello @mantwih ,
A typical issue that can explain this is a bad alignment between your OSTL version (At the moment I write this message we are at OSTL 4.1) and the CubeFWPackage you use (At the moment I write this message, we are at STM32VCube_FW_MP1_1.6.0).

Can you first double check the version of both your A7 soft and your M4 soft ?

Kind regards,
Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.