Skip to main content
ECaba
Associate II
July 24, 2019
Solved

OpenAMP_TTY_echo, don't compile

Hi, I trying to compile the OpenAMP_TTY_echo example, but I get these a lot of errors, attach a file.

This topic has been closed for replies.
ECaba
ECabaBest answer
Associate II
July 25, 2019

Hello, I can compile the examples, I reintalled all: virtual machine, workbench and examples.

Thanks.

3 replies

PatrickF
ST Employee
July 24, 2019

Hello,

Adding more information on your environment (platform, tools) could help. Such kind of compilation issues might have many root causes.

Is your installation correctly compiling other STM32MP1 projects ? if not maybe check again SW4STM32 installation (https://wiki.st.com/stm32mpu/wiki/STM32-CoPro-MPU_plugin_release_note).

Try to remove and re-import again the example project in SystemWorkbench.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
ECaba
ECabaAuthor
Associate II
July 24, 2019

Hello, I using a virtual machine with Ubuntu 18.04.2, I use install_sw2stm32_linux_64bits-V2.9.run to install Workbench and en.stm32cubemp1_v1-0-0.zip to install libraries and examples, my board is STM32MP157C-DK2

I try to import and compile GPIO_EXTI example but I get a lot of errors too, for example:

.../STM32Cube_FW_MP1_V1.0.0/Drivers/STM32MP1xx_HAL_Driver/Src/stm32mp1xx_hal.c: 817:66: error: unknown type name 'uint32_t'

Why don't recognize uint32_t type?

I try to install Workbench with your link.

Thanks.

ECaba
ECabaAuthorBest answer
Associate II
July 25, 2019

Hello, I can compile the examples, I reintalled all: virtual machine, workbench and examples.

Thanks.