Skip to main content
Associate
May 9, 2024
Solved

OP-TEE Trusted Application examples fail to run on STM32MP157F-DK2

I'm attempting to run an OP-TEE Trusted Application on the STM32MP157F-DK2 running OpenST Linux version stm32mp1-openstlinux-6.1-yocto-mickledore-mp1-v23.06.21. I've followed the guides here and here, but both end up producing the following error when attempting to run the application:

TEEC_Opensession failed with code 0xffff0008 origin 0x3

What could be causing this problem? I'm running a fresh install of OpenST Linux and haven't made any modifications to the system other than those required to get the example running.

This topic has been closed for replies.
Pavestone7762Best answer
Associate
May 13, 2024

I found on this page that OP-TEE user trusted applications are disabled by default for ecosystem release v5.0.0. (It would have been helpful for this to be documented on this page as well...)

1 reply

Pavestone7762AuthorBest answer
Associate
May 13, 2024

I found on this page that OP-TEE user trusted applications are disabled by default for ecosystem release v5.0.0. (It would have been helpful for this to be documented on this page as well...)